Is that a open source project with STEVAL-MKI109V3 ?
Posted on February 09, 2018 at 07:39Hi SIR Last days, i got a custom motion sensor board based on STM32F401RE
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on February 09, 2018 at 07:39Hi SIR Last days, i got a custom motion sensor board based on STM32F401RE
Posted on January 25, 2018 at 12:52When the Sensor tile is hooked to Expansion board, the FP ALL MEMS firmware and the custom firmware is able to stream the audio data to STBlue MS app. However the above said firmware would stream noisy data when th...
Posted on February 09, 2018 at 15:20Hi all,I have been working on H3LIS331DL sensor. I am missing one clarification from datasheet of H3LIS331DL.On Page 10 of datasheet H3LIS331DL, Turn on time should be 1/ODR + 1ms.It is clear that based on ODR rat...
Posted on February 05, 2018 at 19:54Hi ALL, I bought the LIS3DH development kit.I want to use it as a sensor that will wake my MCU with interrupt when someone moved my board or tilt it.I have some constrains:1. I need low consumption current with my...
Posted on February 09, 2018 at 10:31Hello, in the LSM303AGR datasheet a low esr capcitor (220nF) is requested on pin5. But no more indication are given.On which frequency the esr must be < 200mOhm ?Thanks for the help.#lsm303agr
Posted on November 01, 2017 at 18:16I have an LIS2DH device in my design and it's working - sort of. I was given some LIS3DH C driver code which I'm using under the advice that the LIS2DH is register-compatible with the LIS3DH.So my requirement is ...
Posted on February 06, 2018 at 09:55Hi,I am looking to test if the interrupt 1 and 2 are working correctly on a LIS2DH.Is it possible to trigger interrupts with the self test functon ?Thank you for the help#lis2dh #self-test #interrput
Posted on February 08, 2018 at 11:36A sensor which can measure soil nutrient values like nitrogen, phosphorus, potassium and can able to connect with ST.
Posted on March 08, 2017 at 10:53Hello all,I want to use ♯ with internal RC oscillator. When I started using ♯ , I prepared a communication library that works well without using the internal RC oscillator. I checked all communication using oscillosc...
Posted on January 25, 2018 at 07:22Hey there, We are working with NUCLEO-F401RE board and are looking forward to interface the imu sensor by Bosch (BMI 160) which contains gyro + accelerometer. wanted to know if there is a sensor fusion library for ...