MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

''VL53L1X GUI'' bug??

Posted on April 26, 2018 at 15:26Hi friends,I have detected a strange problem.The first calibration I apply to VL53L1X sensor is not functional (the measure goes bad). After this, when I apply a new calibration, the measure is right.Has anyone had t...

Accelerometer selection for vibration analysis

Posted on May 05, 2018 at 08:01Hello, we are building an application for condition monitoring of machines. For this, I am trying to figure out the appropriate accelerometer with the following specs: (1) a frequency response of 1.5 to 2 kHz, (2) a hi...

Nucleo STM32L053R8 and bluetooth IDB04a1

Posted on May 09, 2018 at 13:08Hi!I would like to know if there is an example project in which are used two nucleo STM32L053R8 communicating by bluetooth IDB04a1. One board acts as a slave and passes data from the expansion board IKS01A1 to the othe...

Configure LIS2DH for both single click and double click

Posted on May 08, 2018 at 09:52Hello, I want to configure LIS2DH for generating interrupt for single click as well as double click, Can we do that? I am using INT1 for FIFO so INT2 is for clicks interrupt, Individually I can able to get interrupt fr...

X-CUBE-MEMS1 licence requirements?

Posted on May 08, 2018 at 02:56I started a project using the #osxMotionAR library which required a license from ST. This software has been moved into #X-CUBE-MEMS1 together with other osxMotionxx libraries. Is a software licence fro ST still require...

VL53L0X Time-of-Flight Distance Sensor ''FOV''?

Posted on April 11, 2018 at 09:45The specifications of the sensor states a 'FOV of 25 degrees'. I'm not really sure what that FOV means here. The beam is reflected back to the detector and filtered by a pinhole. There's a pinhole, so what would be t...

Resolved! VL53L0X Calibration Target - What to use?

Posted on March 24, 2018 at 14:24The user manual mentions using one 88% reflectance target and 17% reflectance target for calibration. I don't know what material has those reflectance values. What exactly should I use for calibration and where can I...

Josh Yu by Associate II
  • 4157 Views
  • 4 replies
  • 0 kudos

Is it possible to set minimum detectable range? VL53L0X

Posted on April 30, 2018 at 23:44Hi, Is it possible to set minimum detectable range for VL53L0X? I have an application with some parasitic reflections in 10cm zone which I want to ignore. Is it possible to set the detectable range for VL53L0X?

VL53L0X modifiy problem

Posted on April 12, 2018 at 16:25Hi there, I'm new at this form.I'm trying to use VL53L0X api with STM32F103VB cpu. But ı have a big problem. When ı try to use this api keil show windows.h include problem. When ı try this header to comment it sho...

github.com

Posted on April 25, 2018 at 19:02disappointing VL53L0x multiple sensors driver Hello,I got a st VL53L0X shield from ST, and for any people who needed some code, I wrote some faste code here:https://github.com/h2mille/les-beffroyables/tree/master/t%...