MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About VL53L0x

Posted on April 30, 2018 at 09:30Hi All,In my project, It has a cover above VL53L0x( about 5 cm). I want to know what kind of material that the VL53L0x will not to be disturbed by it.It means VL53L0x can work well when a cover above it.Thanks a lot....

VL6180X setting for specular/glossy reflecting targets?

Posted on May 07, 2018 at 12:05Hello,I have to perform some distance measurements in a system of stainless steel pipes. The VL6180X sensor I am using so far gives me values about 10mm below the true distance value.My assumption is that the non-diffu...

LIS3DH Acceleration data calibration

Posted on May 04, 2018 at 11:11I am workeing with LIS3DH sensor ,Configured as normal mode with 2g .I am reading raw data please can any one help me to get the calibration of the X Y Z axesthanks

Resolved! LIS3DH temperature sensor when supply voltage is 1.8V

Posted on May 02, 2018 at 18:10Hello,I have a question regarding a note in the datasheet of the LIS3DH accelerometer:I want to use the accelerometer LIS3DH for one of my application with the following specifications:- The accelerometer is supplied a...

L CO by Associate
  • 1162 Views
  • 2 replies
  • 0 kudos

LIS3DH with strange output values

Posted on February 02, 2018 at 19:40Dear all,        For one important project i need to detect the human falls. I am using the LIS3DH accelerometer configured as the following manner:          CTRL_REG1=0x77 //ODR=400 Hz, high-resolution mode/norma...

magnetic rms noise of the LSM9DS1

Posted on April 16, 2018 at 23:37What is the magnetic rms noise of the LSM9DS1? I can not find it or something simular in the datasheet. Thanks for your help.#magnetic-rms-noise

Ralf L. by Associate
  • 1341 Views
  • 3 replies
  • 0 kudos

Accelerometer MEMS in various ''accelerometer'' chips

Posted on April 26, 2018 at 17:17Dear community,I was just wondering if there was any way of knowing (or whether this is 'secret recipe') whether the very-MEMS within different chips are the same or not.Namely, I would like to know whether I should ...

Operating VL53L1x in histogram mode

Posted on March 14, 2018 at 19:31Dear all,We are interested in reading out time-of-flight histograms from the VL53L1X to explore the application potential for SPAD technology for medical and cosmetic mass-market applications. The device appears to h...

VL53L1x - gesture recognition

Posted on April 26, 2018 at 08:11Hi,Anyone know how to config VL53L1x to gesture recognition? In datasheet is information about support 1D gesture recognition, but nowere I cannot find information how to config it to gesture recognition and how to u...