MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How does LIS3DH configure automatic sleep and arousal?

Posted on March 16, 2018 at 11:40 I want to be able to when the device has detected movement, LIS3DH to wake up from sleep mode, and at a higher rate to detect more than I get a set of threshold, then the interrupt, to remind me of the MCU. I trie...

? ?_3 by Associate II
  • 1864 Views
  • 9 replies
  • 0 kudos

Resolved! Unable to get SensorTile working

Posted on March 04, 2018 at 10:22Hello,I have a SensorTile Kit (STLKT01V1) that I'm trying to test with the Blue MS Android application.As mentioned in the SensorTile http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/bc/b1...

MEMS (NIR)

Posted on March 31, 2018 at 18:39Hi I am currently working on a project with MEMS Sensors (Near Infrared Sensors between 1and 5 micrometer wavelenght), I am no Expert and my challenge is to evaluate user benefits and find application fields e.g. The...

LSM303C communication to microcontroller via 3-wire SPI

Posted on June 19, 2015 at 09:09I am interfacing LSM303C magnetometer and accelerometer to microcontroller via 3-wire SPI, where SIMO and SOMI from uC are connected together via R 10k to allow the slave LSM303C to drive this single signal line when ...

pljushev by Associate
  • 828 Views
  • 2 replies
  • 0 kudos

What is PDM format?

Posted on March 17, 2017 at 17:25Hello,I want to use MP34DT01 microphone in our application. But data stream format is unclear. Explain this please. I guess this is the usual delta modulation. Is not it? Analog Devices for ADMP521 was describe it tr...

X-NUCLEO-53L0A1 with Nucleo F030R8

Posted on August 10, 2016 at 16:46Hy,what would be the easiest way to use the VL53L0X Nucleo Expansion board (X-NUCLEO-53L0A1) with Nucleo F030R8?All given examples rely on a F401, the source code would not work immediately, because there are some f...

harald by Associate III
  • 956 Views
  • 1 replies
  • 0 kudos

F401RE VL53L1X debug issue

Posted on March 21, 2018 at 15:51Hello,i'm quite new to the embedded world and purchased the VL53L1X evaluation kit with the F401RE and thehttp://www.st.com/en/ecosystems/x-nucleo-53l1a1.html. I installed all the drivers and the System Workbench on ...

LIS3DH

Posted on March 07, 2018 at 14:03Hi Sir,I am using ST accelerometer Sensor  LIS3DH (adapter board STEVAL-MKI105V1) with I2C interface.I can now read the registers. But for the registers which doesn't have default value, for example,OUT_X_L (0x28),OU...

Arna Lee by Associate II
  • 2052 Views
  • 7 replies
  • 0 kudos