MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM330TR GYRO power_down mode

Posted on June 21, 2018 at 06:58Hi, I'm in trouble about LSM330TR gyroscope power_down mode.I'm measuring the angular velocity every 100ms and when it isn't measuring, i'd like to implement power_down mode.I wrote such a program but the gyro data is...

LV53L0X outside

Posted on June 17, 2018 at 21:30are there any settings or lenses for the LV53L0X to help it cope with high ambiant light?#lv53l0x #outside

VL53L0X_SetVcselPulsePeriod?

Posted on June 21, 2018 at 19:54is there any information of any type regarding the funktion   VL53L0X_SetVcselPulsePeriod how do i use it in other ways then what is in the API note?

Wrong result from MotionFX

Posted on June 21, 2018 at 14:18Hello,I'm trying to get run the MotionFX library using STM32L4 and SensiBLE board (which is equivalent to Nucleo-L476RG + X-Nucleo-IDB05A1 + X-Nucleo-IKS01A1 + X-Nucleo-CCA02M1).The module for the accelerometer and gy...

VL53L1 Accuracy Issue

Posted on June 19, 2018 at 14:12HiWe have interfaced VL53L1 to STM32L0 EVM board(B-L072Z-LRWAN1).We tested the sensor with a white surface and water in opaque object.The accuracy with white surface are good if the object is below 200cm.If above 200c...

Where to find VL53L1x window cover?

Posted on June 10, 2018 at 20:50I need an outdoor window cover for the ToF VL53L1X. I�m planning to use it as a people detector sensor. I want to put it into an abs plastic case.Here is the module that I obtain from Pololuhttps://www.pololu.com/prod...

Resolved! LIS3DE vs. LIS3DH HW FIFO Handling

Posted on June 11, 2018 at 14:55Hello,we've been using the LIS3DH on a development board and have switched to the LIS3DE for the prototype. We're using the HW fifo feature to batch-read values from the sensor. The LIS3DE is only 8-bit and thus I was...

Resolved! What is the silicon square on the LPS22HB and LPS25HB?

Posted on June 18, 2018 at 11:17In section 10.1 of the datasheet for the LPS22HB the square on top of the package is labelled as 'Sensing area (exposed silicon)', which makes it sound quite fragile.  However I noticed in a recent press release: http...

mart J by Associate II
  • 1732 Views
  • 4 replies
  • 0 kudos