MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X interrupt setting

Posted on May 21, 2018 at 06:53Hi  I am trying to get the VL53L0X using the api provided and the source code available on https://os.mbed.com/users/andcor02/code/vl53l0x_api/  which is just a copy of the VL53L0X api. I am using the STM32L432KC NUCLE...

When will the VL53L1X API source code be available

Posted on March 13, 2018 at 09:31The default application http://www.st.com/content/st_com/en/products/embedded-software/proximity-sensors-software/stsw-img008.html doesn't allow to use the multi-zone feature mentionned in this http://www.st.com/cont...

Resolved! Wrong answer to LSM6DS3 Who-Am-I register

Posted on June 11, 2018 at 14:40I have a weird problem with LSM6DS3. Right after power on I try to read the Who Am I register, via SPI. The return value is 0xFF, if I read it again it will send the correct value 0x69.In other words, in order to get ...

LIS3DH Activity/Inactivity detection

Posted on May 17, 2017 at 21:36This document http://www.st.com/content/ccc/resource/technical/document/application_note/77/ed/e7/e1/28/5a/45/d6/CD00290365.pdf/files/CD00290365.pdf/jcr:content/translations/en.CD00290365.pdf provides information rega...

Run VL53L0X at lower voltage than specified?

Posted on June 11, 2018 at 14:37Hi, the specifications of the  VL53L0X said that recommended input voltage is between 2.5 and  3.5VI have test it on a prototype at 2V and works fine at short range  (150 mm).  Which problems can i experience? If the ...

LIS2HH12 sensor output data

Posted on May 27, 2018 at 11:00Hello,we have connected the lis2hh12 accelometer with our linux board using i2c bus. I am ableto read the raw x,y,z values from sensor using sysfs interface. How can i convert these raw values to actual acceleration(m/...

[SOLVED] LIS3DH on I2C: setting Activity Interrupt

Posted on June 09, 2018 at 11:44[EDIT] Solved!  I missed where the app note mentioned that I have to set REG3's <I1_IA1> bit.  Once that's done, I get interrupts on motion.'App Note AN3308'Hello,I'm trying to enable interrupt on a LIS3DH using mBED,...