Posted on June 11, 2018 at 14:37Hi, the specifications of the VL53L0X said that recommended input voltage is between 2.5 and 3.5VI have test it on a prototype at 2V and works fine at short range (150 mm). Which problems can i experience? If the ...
Posted on June 08, 2018 at 13:37I have been using the LIS3MDL with the ST breakout board and seems that the Latch interrupt request in the register INT_CFG (30h) has the description wrong.From my tests : 1: interrupt request latched; 0: interrupt re...