MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

In HTS221 sensor not getting correct Humidity data

Posted on September 22, 2015 at 08:14I am using HTS221 , and I am taking value from HTS221 via I2C.Here i was successful to get correct temperature data you can see in attach .txt file.But for Humidity i am getting values but they are not as per env...

jayesh1 by Associate
  • 3139 Views
  • 5 replies
  • 0 kudos

Begining with LIS3DHTR Sensor for tap detection

Require some basic knowledge to use LIS3DHTR https://store.ncd.io/product/lis3dhtr-3-axis-accelerometer-digital-output-motion-sensor-i2c-mini-module/ to work with arduino and make the TAP detection solution but to make it work. As beginner in this, I...

Resolved! LIS2HH12 - Meaning of RES pin

Hello,I have a board on my desk where the RES pin (#5) of LIS2HH12 is not connected.The data sheet says, Connect to GND. OK ... not good ...As I do not get any response of the accelerometer via I2C, I would like to know if this pin is the reason. I c...

s m by Associate III
  • 2139 Views
  • 3 replies
  • 0 kudos

Failure reading from LIS3DSH SPI interface

I am interfacing a LIS3DSH using SPI. My MCU is a Texas Instruments MSP432.When writing and checking configuration registers, even-addressed ones do not return the expected value.After sending a byte, MSP432 MOSI retains the value of its MSB. This is...

0690X000006C44SQAS.png 0690X000006C3yoQAC.png 0690X000006C3z8QAC.png 0690X000006C3zSQAS.png
GioP by Associate II
  • 955 Views
  • 0 replies
  • 0 kudos

MEMS measurement ranges hardware details

Hello everyone,How does MEMS measurement ranges realized in hardware in details? Does it use: 1. Amplifiers with different gain ratios? 2. ADC with as many bits as need to serve maximal range with minimal resolution? 3. Does different MEMS cells used...

LIS3MDL Magnetometer data reading Error

Hi All,I am working on the LIS3MDL register on my board. But When I try to measure the Magnetic field Produced by motors, I am getting very high deviation.My settings for the LIS3MDL are as below.0x22 -- 0x00 (also tried with 0x22 -- 0x03)0x21 -- 0x0...

HGohe by Associate II
  • 4845 Views
  • 8 replies
  • 0 kudos

STMPE610 - cant read data

im using the feather nrf52832 with the featherwing.i can read the ID by sending 0x00 as [0x80,0x81,0x00] = getting 0x0811i tried to do the same with TSC_DATA_X 0x4D , but i can read any data from the sensor.my init is :  writeRegister8(SYS_CTRL2, 0x...

ykein by Associate
  • 903 Views
  • 0 replies
  • 0 kudos

VL53L1x factory default ?

Since there's no information on the registers in the datasheet, and half of the API is in the documentation. I'd like to know if there's a reset/factory default settings for the chip ?I was building the platform file and sent a lot of crap to the dev...

SBeno by Associate
  • 924 Views
  • 0 replies
  • 0 kudos

Would like to receive audio stream from Sensor Tile board

Hello,I have STEVAL-STLKT01V1 sensortile board and would like to stream the audio from sensortile board to raspberry pi board via BLE interface.https://www.st.com/en/evaluation-tools/steval-stlkt01v1.htmlFor this, ST provided BlueVoice python framewo...