MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DS33 FIFO watermark interrupt issue

Posted on June 04, 2018 at 23:53Good day everyone!I am trying to use a FIFO watermark interrupt on LSM6DS33 accelerometer. For some reason, the interrupt doesn't happen. Other interrupts (Free-fall, movement, significant motion) work just fine, so i...

How to design a High Speed data logger?

Posted on June 04, 2018 at 15:13Hai, I want to build a data logger attached to an object travel at 3m/s. The requirement is the data logger must capture 74 sensor input (10 bit ADC) at every 3mm along the travel path. Thus in 1 second, the data logg...

Sensor Tile Linear Acceleration

Posted on June 02, 2018 at 10:08Hi ThereI recently got the STEVAL-STLKT01V1 sensor tile evaluation kit. I know that some of the sensors on the sensor tile are able to record linear acceleration (LSM303AGR). I have been looking at the provided exampl...

HTS221 I2C STOPS WORKING

Posted on June 13, 2016 at 07:51Hi, I'm using the HTS221 with STM8L052C6. The communication channel is I2C. I am able to get the humidity data upto 99% RH. but above this after some point of reading the data,the sensor gets hanged and is not recover...

unnati811 by Associate II
  • 1094 Views
  • 4 replies
  • 0 kudos

STM32 Cube and ADXL345 ACC

Posted on May 31, 2018 at 13:46Hi,I am trying to use STM32 cube and ADXL345 ACC using SPI , this is my first time trying , and currently without luck as i am not able to read the accelerometer This is my SPI init code :void MX_SPI1_Init(void){hspi1....

[ATT]11840

Posted on April 06, 2018 at 01:33SensorTile: Auto Log on power-upAll:I have been tinkering with the SensorTile to use as-is for some data logging applications.  It wasn't my original intent, but it turned out to be so handy as-is I didn't see a need...

willcfj by Senior
  • 1823 Views
  • 1 replies
  • 0 kudos

Accelerometer Reading Issue

Posted on May 14, 2018 at 15:01Hi There, I am using the STM Accelerometer(LIS2DE12) with STM(stm32l432kb) controller. While getting the readings from the Accelerometer it gives the random value continuously. Even it shows false value at steady posit...

K_P_D by Associate II
  • 2584 Views
  • 12 replies
  • 0 kudos

Resolved! Best Approach Using the LIS3DSH Accelerometer?

Posted on May 27, 2018 at 18:12Hi, I'm using an LIS3DSH in a case where I want to periodically (say once every 50 milliseconds) get the most recent X,Y,Z position of the accelerometer and perform a calculation.My current approach is to just set a ti...

NXT

Posted on May 28, 2018 at 18:14I am designing a robot using LSM6DSL.   I have it mounted in my system and trying to program.    Regarding the device's offset from the center of my machine.  Is there a simple register we can program with a simple phy...

Hello, We are carrying out experiments using lis3dsh accelerometer. With ODR set to say, 50Hz and INT1 enabled, we are seeing the INT1 coming at ~48Hz instead of 50Hz We are unable to find any document on internal clock spec It would help if we could som

Posted on May 28, 2018 at 16:17Please find the register settings as below NameAddressValueCTRL_REG30x230XE8CTRL_REG4,0x200X67CTRL_REG50x240XC0CTRL_REG60x250X10FIFO_CTRL0x2E0X0