cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, We are carrying out experiments using lis3dsh accelerometer. With ODR set to say, 50Hz and INT1 enabled, we are seeing the INT1 coming at ~48Hz instead of 50Hz We are unable to find any document on internal clock spec It would help if we could som

MARIA XAVY
Associate
Posted on May 28, 2018 at 16:17

Please find the register settings as below

NameAddressValue

CTRL_REG3

0x23

0XE8

CTRL_REG4,

0x20

0X67

CTRL_REG5

0x24

0XC0

CTRL_REG6

0x25

0X10

FIFO_CTRL

0x2E

0X0

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0