MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

More info on MotionMC function MotionMC_SaveCalInNVM

Dear Community,​I've been using the MotionMC library on a stm32f401 with quite some succes, but there are 2 functions that remain somewhat mysterious:char MotionMC_LoadCalFromNVM(unsigned short int datasize, unsigned int *data);andchar MotionMC_SaveC...

Léon by Associate
  • 1680 Views
  • 2 replies
  • 0 kudos

USB Device HS-IN-FS does NOT work

I am using STM32Cube_FW_F4_V1.21.0.This is very excellent software.UART,SPI,I2S,RTC,,,work fine but HS-IN-FS.I have checked HS and FS works fine.My target board is STM32469I-EVAL board and I'm using EWARM compiler suite.My application is USB_Device/M...

TKawa.17 by Associate
  • 808 Views
  • 0 replies
  • 0 kudos

VL53L0X Sensor Communication(Failed reach)

I bought vl53l0x sensor in mouser.I designed in my sensor board for my project. I refered in datasheet circuit.I added my board schematics.İn addition to ı constructed to ı2c level shifter with mosfet for the arduino communication but i did not answe...

LIS3DH Power-Down Mode

On my custom board LIS3DH is supplied with Vdd = Vdd_IO = 3.3 V and is driven through I2C digital interface.On power-on LIS3DH, after its boot sequence (5 ms) should be automatically configured in power-down mode with a current consumption less then ...

Vagni by Associate III
  • 3010 Views
  • 3 replies
  • 0 kudos

Range setting in ISM330DLC

Hi All,I am working on a project that is using ISM330DLC sensor for measuring the acceleration along the X,Y and Z-axis. When I set range 2G,4G and 8G I'm seeing difference in the sensor raw value and when I set it to 16G, I'm getting same data as 8G...

LSM6DSl edge-sensitive trigger mode

Hello,I want to use edge-sensitive trigger mode to synchronize multiple sensors. In the code snippet you can see the relevant code for that. The FIFO buffer doesn't get filled, even though I have a PWM as trigger on the INT2 pin. The low-pass filter ...

RHube by Associate
  • 1542 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.