MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lis2dw12 sensor SPI CPHA and CPOL setting

Hi all,I'm using lis2dw12 sensor and interfaced with SPI. In which SPI mode i can get proper data from the sensor?CPHA = 0, CPOL = 0;CPHA = 0, CPOL = 1;CPHA = 1, CPOL = 0;CPHA = 1, CPOL = 1;Thanks and regards,Basavanagouda

VL53L1X readings unreliable when no object in front

I am testing the VL53L1X in medium measurement mode at 200ms timing budget I get 140cm weak return signal value even when there is no object in front.In long measurement mode with 300ms timing budget with no object infront the values I get are jitter...

AKhan.15 by Associate II
  • 821 Views
  • 0 replies
  • 0 kudos

LSM303C Accelerometer Activity/Inactivity Interrupt

Hi,This question was asked by someone 4 years ago and hasn't been answered yet. Hope it gets answered this time around.I have been trying to experiment with the interrupt functionality of LSM303C with no success.So far I have followed all the steps i...

SLokh by Associate
  • 748 Views
  • 0 replies
  • 1 kudos

Do the LIS3MDL Reserved Pins need to be connected?

Hi, we have a board with several I2C based sensors on it, including the LIS3MDL and LIS3DH.The 3DH works like a treat, but I cant get any communication from the 3MDL. The only thing I can see that would cause this is a discrepancy with our board desi...

JRule by Associate
  • 1809 Views
  • 6 replies
  • 0 kudos

power down L3g20h

Hello.I'm working with a l3gd20 to detect an angular movement but most of the time the mic is asleep and to save energy I want to put the l3gd20 into low consumption, for that I am writing to CTRL_REG1 0x00 to be in power down but the gyro does not h...

fagui by Associate
  • 1086 Views
  • 3 replies
  • 0 kudos

Enable LSE oscilator in sensortile

Hello, I am using sensortile with my own PCB. But some sensortiles doesn't work. I am trying to build sensortile sample code and it can't enable LSE oscilator.Thanks for your helpHave a nice day

DVALL.9 by Associate
  • 581 Views
  • 0 replies
  • 0 kudos