Skip to main content
David T_2
Associate
June 27, 2018
Question

LSM303AGR and int1

  • June 27, 2018
  • 1 reply
  • 858 views
Posted on June 27, 2018 at 11:09

With the next configuration, the INT1 don't start.

Base on (

https://github.com/STMicroelectronics/STMems_Standard_C_drivers/tree/master/lsm303agr_STdC

)

lsm303agr_xl_operating_mode_set(&dev_ctx_xl, LSM303AGR_XL_POWER_DOWN);

lsm303agr_ctrl_reg3_a_t int1_config;

int1_config.i1_aoi1 = 1;

int1_config.i1_aoi2 = 0;

int1_config.i1_click = 0;

int1_config.i1_drdy1 = 0;

int1_config.i1_drdy2 = 0;

int1_config.i1_overrun = 0;

int1_config.i1_wtm = 0;

int1_config.not_used_01 = 0;

lsm303agr_xl_pin_int1_config_set(&dev_ctx_xl, &int1_config);

lsm303agr_xl_high_pass_int_conf_set(&dev_ctx_xl, LSM303AGR_DISC_FROM_INT_GENERATOR);

lsm303agr_xl_full_scale_set(&dev_ctx_xl, LSM303AGR_2g);

lsm303agr_xl_int1_pin_detect_4d_set(&dev_ctx_xl, 0x08);

lsm303agr_ctrl_reg6_a_t int2_config;

int2_config.h_lactive = 1;

int2_config.boot_i2 = 0;

int2_config.i2_clicken = 0 ;

int2_config.i2_int1 = 0;

int2_config.i2_int2 = 0;

int2_config.not_used_01 = 0;

int2_config.not_used_02 = 0;

int2_config.p2_act = 0;

lsm303agr_xl_pin_int2_config_set(&dev_ctx_xl, &int2_config);

lsm303agr_xl_int1_gen_threshold_set(&dev_ctx_xl, 0x04);

lsm303agr_xl_int1_gen_duration_set(&dev_ctx_xl, 0x04);

lsm303agr_int1_cfg_a_t int_1_cfg;

int_1_cfg.xlie = 0;

int_1_cfg.xhie = 1;

int_1_cfg.ylie = 0;

int_1_cfg.yhie = 1;

int_1_cfg.zlie = 0;

int_1_cfg.zhie = 1;

int_1_cfg._6d = 0;

int_1_cfg.aoi = 0;

lsm303agr_xl_int1_gen_conf_set(&dev_ctx_xl, &int_1_cfg);

lsm303agr_int1_src_a_t int_source_get;

lsm303agr_xl_int1_gen_source_get(&dev_ctx_xl, &

int_source_get

);

lsm303agr_xl_data_rate_set(&dev_ctx_xl, LSM303AGR_XL_ODR_50Hz);

WhoamI return correct value. 

I work with a NRF52,

For read the pin i

nterrupt

:

ret_code_t err_code;

err_code = nrf_drv_gpiote_init();

APP_ERROR_CHECK(err_code);

nrf_drv_gpiote_in_config_t in_config = GPIOTE_CONFIG_IN_SENSE_HITOLO(false);

in_config.pull = NRF_GPIO_PIN_PULLUP;

err_code = nrf_drv_gpiote_in_init(INT_1, &in_config, in_pin_handler);

APP_ERROR_CHECK(err_code);

nrf_drv_gpiote_in_event_enable(

INT_1

, true);

The 'in_pin_handler' never called.

#int1 #lsm303agr #interrupt
This topic has been closed for replies.

1 reply

David T_2
David T_2Author
Associate
June 27, 2018
Posted on June 27, 2018 at 16:47

With this config work fine:

lsm303agr_xl_block_data_update_set(&dev_ctx_xl, PROPERTY_ENABLE);

lsm303agr_xl_data_rate_set(&dev_ctx_xl, LSM303AGR_XL_ODR_100Hz);

lsm303agr_xl_full_scale_set(&dev_ctx_xl, LSM303AGR_2g);

lsm303agr_xl_operating_mode_set(&dev_ctx_xl, LSM303AGR_LP_8bit);

lsm303agr_xl_high_pass_int_conf_set(&dev_ctx_xl, 0x01);

lsm303agr_xl_high_pass_on_outputs_set(&dev_ctx_xl, 0x01);

lsm303agr_ctrl_reg3_a_t reg3_confg;

reg3_confg.i1_aoi1 = 1;

reg3_confg.i1_aoi2 = 0;

reg3_confg.i1_click = 0;

reg3_confg.i1_drdy1 = 0;

reg3_confg.i1_drdy2 = 0;

reg3_confg.i1_overrun = 0;

reg3_confg.i1_wtm = 0;

reg3_confg.not_used_01 = 0;

lsm303agr_xl_pin_int1_config_set(&dev_ctx_xl, &reg3_confg);

lsm303agr_xl_int1pin_notification_mode_set(&dev_ctx_xl, LSM303AGR_INT1_PULSED);

lsm303agr_xl_int1_gen_threshold_set(&dev_ctx_xl, 0x08);

lsm303agr_xl_int1_gen_duration_set(&dev_ctx_xl, 0x00);

lsm303agr_xl_high_pass_mode_set(&dev_ctx_xl, LSM303AGR_AUTORST_ON_INT);

lsm303agr_int1_cfg_a_t int1_config;

int1_config.xlie = 0;

int1_config.xhie = 1;

int1_config.ylie = 0;

int1_config.yhie = 1;

int1_config.zlie = 0;

int1_config.zhie = 1;

int1_config._6d = 0;

int1_config.aoi = 0;

lsm303agr_xl_int1_gen_conf_set(&dev_ctx_xl, &int1_config);