MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STEVAL-MKI109V3 Dfuse update issue

Hello,I am trying to get the STEVAL-MKI109V3 upgraded to support the STEVAL-MKI179V1.When I first tried to use the 109V3, Unico said my firmware was out of date and needs to be updated to support the 179V1.So I used Dfuse to update the part. I am usi...

0690X000006CDSrQAO.png 0690X000006CDSwQAO.png
LCorb by Associate
  • 502 Views
  • 1 replies
  • 0 kudos

LPS22HB as pressure sensor

I try to use the LPS22HB as real pressure sensor (measure of force against the skin, but I almost didn't see any change. Only when press with big force I see the change.Does the name of barometer mean it can't sense pure pressure against its window?

Barbie by Associate II
  • 1421 Views
  • 5 replies
  • 0 kudos

LPS33HW SW & EV board

If I want to test the LPS33HW and I already have the X-NUCLEO-IKS01A2 motion MEMS place over STM32 Nucleo test by DataLogTerminal SW from X-CUBE-MEMS1 package.I see there is LPS33HW EV STEVAL-MKI183V1. But I didn't see any reference to use it on the ...

Barbie by Associate II
  • 708 Views
  • 1 replies
  • 0 kudos

LIS2DH not responding with any data

I'm having a nightmare trying to get my LIS2DH to respond. SA0 is high, CS is high.It kind of responds to the right address (others get nothing), but data is all zeros.All I want to do is get XYZ data out, these are all zeros too!The I2C timing chart...

0690X000006CEldQAG.png

VL53L1X range readings not accurate after 200cm

We are testing VL53L1X Time of Flight Sensor with STM32L072(B-L072z-Lrwan) controller. Within 200cm the range measured by sensor is accurate. After 200cm we are getting a lot of variation in the range is measured by the sensor. We have to change the ...

Resolved! LSM303AGR can't enable temperature sensor

I am having a problem when initializing temperature sensor on LSM303AGR. To simplify everything for a test I am using direct commands. Writing 0xC0 to register 0x1F and then reading back register 0x1F results in 0x00 reply instead of 0xC0. Why is it ...

MHuk by Associate II
  • 684 Views
  • 1 replies
  • 0 kudos

LSM6DSL - values not correct

Hi :) i m using LSM6DSL accelometer . i My sensivity is -2g/+2g. I have 16 bit (65535 values ) . Well, when i take values, i have values as: 65,423- 64,912 - 16,076325 - 61,613 - 58448 I dont undestand this value. I think 16,076 is 1 g...