MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L0X single ref calibration error

Posted on December 04, 2017 at 15:52 Hello, i want to use the VL53L0X sensor with an ARM processor. For that purpose I took the Pololu Arduino library, rewrote the i2c part and everything worked fine. My problem with the Pololu librays is that...

VL53L1X GUI Connection failure

Hello,I am using Windows 7 Ultimate and have the same problem that community member dconrad has already described very well. (see link).In addition, I noticed the following:When the GUI is runing, the red glowing double LED LD1 on the board, flashes ...

Markus1 by Associate
  • 507 Views
  • 0 replies
  • 0 kudos

X-NUCLEO-CCA02M1 not recognized as sound device on PC

Posted on October 12, 2017 at 03:53Hi,I am testing X-NUCLEO-CCA02M1+NUCLEO-F401RE by following below instruction (page 7-9).http://www.st.com/content/ccc/resource/sales_and_marketing/presentation/product_presentation/d3/44/de/b9/33/a0/4e/25/x-nucleo...

VL53L0X SPAD setup

I see in the documents for the VL53L1X the SPAD grid is labeled out. Is this the same grid labeling for the L0X? How does this grid work? For instance, does it grow as the cone does with further measurements? Thanks

ADike by Associate
  • 558 Views
  • 0 replies
  • 0 kudos

VL53L0X: Cone at Distance X - Objects in way

Posted on May 26, 2018 at 15:52My question is about the VL53L0X.In the Datasheet on Page 30, there is a Collector Exclusion and Emiter Exclusion Zone defined. Sadly I did not find any information how big the cone will be at a Distance X. Is this con...

Example acceleration data - LIS3DH

Section 4.2.3 of the application note for the LIS3DH sensor provides example register values for various sensor readings. For +/-2g at high resolution mode the typical sensitivity is 1mg/unit. When BLE=0, I see why registers 28h and 29h are E0h and 1...

MG by Associate
  • 736 Views
  • 2 replies
  • 0 kudos