MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems using the VL53L0X in a 3D printed tube

I would like to use the VL53L0X in a 3D printed tube with limited space. The diameter is 6,5mm.Since the emitter and collector have a conical characteristic, there are limitations as describes in an earlier post: https://community.st.com/s/question/0...

Ingo1 by Associate
  • 1663 Views
  • 0 replies
  • 0 kudos

SPI Stopped Working

Hi,I'm working with a STM32F401 Nucleo-64 board. The board is connected to a mems accelerometer (IIS2DH) via SPI, and I'm using the HAL library.Everything was working good and I was able to retrieve samples from the accelerometer. Suddenly one day la...

CJoha by Associate II
  • 1961 Views
  • 4 replies
  • 0 kudos

Resolved! Temperature sensor on LIS2HH12 accelerometer

Posted on June 19, 2017 at 20:00We're using the LIS2HH12 accelerometer and there's a temperature sensor listed in the datasheet accessible via the temp_L and temp_H registers (16 bits).However the numbers I get don't make any sense.The datasheet men...

LIS2DH12TR

I'm new to Accelerometer Sensor.I have few questions o this LIS2DH12TR.There are two Interrupt pins on this LIS2DH12TR.The interrupt pins are meant for Threshold detection and sending the LIS2DH12TR to sleep/wakeup mode? Can you briefly explain the f...

LN by Associate II
  • 1156 Views
  • 1 replies
  • 0 kudos

ST MEMS L3GD20 interfacing with STM32F429ZI

Hello, I need help using L3GD20 gyroscope that comes with stm32f429ZI DISC! board. I have used code in this thread as the example and this video to generate code using cube MX/* Includes ---------------------------------------------------------------...

AS Na by Associate II
  • 2028 Views
  • 4 replies
  • 0 kudos

Recovery of Standby Mode in LIS3DH + STM32L072

Recovery of Standby Mode in LIS3DH + STM32L072I am developing using LIS3DH + STM32L072 now.I think that I want to restore with WKUP (PA0) of STM32L072 by INT1 when it enters Standby Mode and exceeds the threshold set to LIS3DH.However, I will not ret...

Interrupt line not being cleared

I'm using an H3LIS331DL chip, and relying on the set threshold to trigger an interrupt and go read the data.Everything is working fine, except occasionally it will freeze and stop reading anything. On investigation, I found the interrupt output line ...

0690X0000087hW1QAI.png 0690X0000087hW6QAI.png 0690X0000087hWBQAY.png 0690X0000087hWGQAY.png
RDyla by Associate II
  • 2027 Views
  • 3 replies
  • 0 kudos

Resolved! What does the DEN_A/G pin on the LSM9DS1 actually do?

Posted on February 10, 2015 at 15:24The title really says it all. The pin description for the LSM9DS1 says that the DEN_A/G pin is the Accelerometer/Gyroscope Data Enable. This sounds important, but I can't see anywhere in the datasheet that explai...

evan2 by Associate II
  • 5724 Views
  • 10 replies
  • 0 kudos