MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSLTR and ESP32 - one axis of gyro is not detecting

 I am currently working with the LSM6DSLTR IMU sensor, interfacing it with an ESP32-S3-WROOM-1-N8R2 using the I2C protocol. However, I have encountered an issue where one of the accelerometer axes is not providing any data.Issue Observed:The sensor i...

Resolved! MEMS Studio and Nucleo Boards

I’m running MEMS Studio 1.4.2 on Win 10, 64 bit latest version. And trying three different Nucleo boards:Nucleo-C031C6Nucleo-64-STM32L476Nucleo-64-STM32F303MEMS Studio will not recognize any of these three Nucleo boards, with or without the MEMS iner...

LSM6DSL INT2 <-> LIS3MDL DRDY short circuit???

I am operating a LSM6DSL with a LIS3MDL in sensor hub mode, where the DRDY pin from the LIS3MDL is connected to the INT2 pin of the LSM6DSL. Basically, it works. However, there is a problem during initialization.In order to configure the LIS3MDL, the...

bbox by Associate
  • 1050 Views
  • 2 replies
  • 0 kudos

Resolved! H3LIS331DL XYZ read out data abnormal

Hello ST Friends,Here we are using H3LIS331DL in our product, using SPI interface. Below is the schematic. and related code is below.    /* Check device ID */ static uint8_t whoamI, tData; whoamI = 0; h3lis331dl_device_id_get(&dev_ctx_xl, &w...

lyan2_0-1741524879538.png lyan2_2-1741525513581.png lyan2_1-1741525449604.png lyan2_3-1741525543158.png
lyan.2 by Associate II
  • 2380 Views
  • 6 replies
  • 3 kudos

How to use interrupt for TSL2591

HiI purchased the TSL2591 product and used it on the STM32 board.I am reading the datasheet and creating the code.I initialized the first writable registers to 0x00.I then looked at the datasheet and gave the control register a value of 0xB0.The conf...

SKim.14 by Associate
  • 2900 Views
  • 5 replies
  • 0 kudos

LSM6DSO not reading 1G at rest

I  am writing my own library in C++ to operate the LSM6DSO and when the sensor is at rest it reads 0.5 G on the z-axis, I've tried the code with 2 ICs, one in an Adafruit breakout board, and another one in an old PCB that had the sensor soldered one ...

Diogo_Goto_0-1739051739233.png Diogo_Goto_1-1739054006872.png Diogo_Goto_2-1739054522593.png

Temperature characteristics of IIS2DLPC

I am making a simple inclinometer using IIS2DLPC. The 'Zero-g offset change vs. temperature' of IIS2DLPC is specified as a maximum of ±1mg/℃, but some of the boards I made have reached 2.93mg/℃.Some have relatively good values ​​of 0.3-0.4mg/℃, while...

t-susaki by Associate II
  • 1853 Views
  • 5 replies
  • 0 kudos