Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, currently, lis3dh is running well with IA1 function, but if i want to change some config, such as CTRL_REG1(20h) for change target axis INT1_CFG(30h) for target axis and direction change INT1_THS(32h) fo...
In the datasheet, it says that LA_TyOff can be eliminated by enabling built-in high pass filter, but for accelerometer, the high pass filter can't be disabled (I assume that the normal mode means high pass filter is enabled, in CTRL_REG7_XM). I had a...
Posted on March 05, 2018 at 16:43Hi,I am a novice trying to work on some sensors by connecting them to the STM32L476 nucleo 64 board. Currently I am trying to use the Time of flight sensor, VL53L0X breakout board, by connecting it at the I2C pins on...
Namely, I want to know the linear acceleration sensitivity of the LSM9DS1 expressed in (m/s^2)/LSB, not in the g/LSB. It is well known that g at the Earth Poles is 9,832 m/s^2, but at the Equator is 9,780 m/s^2.Yes, such few difference is important f...
Hi ,for my new project, we placed two LIS3DSH vibration sensor on one small PCB,and we need to acquire both sensor data simultaneously with different address on same I2C port,Can you give any idea about how to manage two Lis3DSH data aquation on same...
Hi I am using, ST eval (STEVALI109V2),suddenly its not working,its not giving usb port ,when i connected to PC, D1 & D5 LED are blinking,please guide me ,how to fix it.Regards,Chaitanya
Hi, from Data sheet, i saw section 3.5, it says no need to further calibration but when i check output data from register 28-2D, the value is variety time to time , it has variety range for +- 20 ~ +-40, is it correct? or we should do calib...
Hello allI am new at this forum and have almost zero knowledge in electronics but look at acceleration data on a daily basis (in the geophysics field).My experience is that MEMS accelero are quite noisy, especially at "low" frequencies (<~1 Hz).Just...
I am using an H3LIS331DL accelerometer on a custom PCB. I wish to use it to attempt to capture some drop events. Using an analog accelerometer, I have seen that the drop event occurs within approximately 1-1.5 msec. Will this accelerometer be able to...