Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
HelloI want to use the IIS2MDC magnetometer in a device which measures magnetic fields that change rapidly as a function of position (e.g. fields with high gradients). For this purpose, I need to know two things which i couldn't find in the datasheet...
Help me? I don't understand how has obtained vector X (Equation 27-29, page 28-29, AN 3192)?
I am assuming that since they can be configured as push-pull or open drain that they are likely active low, but I would like to confirm this assumption. It seems odd that there is nothing in the datasheet about these pins -- only info about their sof...
Hi,Can I use MEMS libraries such as libMotionAC220_CM4F_GCC_ot.a with STM32F7 and with TrueStudio? as I see these are for CM4. Thanks,
Hi,I am attempting to port the MotionFX Library example to another processor. The project I am using as a reference is the DataLogFusion project for the STM32L476RG-Nucleo in the X-CUBE-MEMS1 V6.0.1. I am trying to compile it on another ARM Cortex M4...
Hello everyone, I'm developing an IoT product with the LIS3DH and I'm thinking about running the self-test regularly this could be anything between 30 minutes and 2 hours; would this kind of behavior impact the life of the sensor? is there any data o...
Though the maximum range of the VL53L1X is 400cm, it gives random readings within 400cm when it is directed to open space. The VL53L0X gives a value about 8.1m for out of range measurements so that we can filter out them. But in VL53L1X there is no w...
Hi all,I am trying to get the VL6180X to work with my TI MSP432P401R Microcontroller. I purchased my VL6180X on a breakout board manufactured by Adafruit (https://www.adafruit.com/product/3316). I have gotten it working with an Arduino just to verify...