cancel
Showing results for 
Search instead for 
Did you mean: 

How may i implement the Harsh Cornering, Harsh Acceleration and Harsh breaking using ST MEMS Lib?

SPate.19
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Eleon BORLINI
ST Employee

Hi, sorry for the delay in the answer. Which device are you using (accelerometer, 6axis...) and which part number? And which is you target application (e.g. is it an automotive application)? You can btw check the X-CUBE-MEMS1 and the related libraries (here). You could in general use the Motion AR library that enables the activity recognition function, but some sensor enables you to develop a Finite State Machine or a Machine Learning to implement the activity recognition. Regards