MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-MEMS1 Middleware initialization problem

Hi,I am using a Nucleo-F446RE board with an IFS01A2 to build an eCompass.I have built a project using CubeMX v5.2.1 and Atollic Truestudio v9.1.To start with I made sure that I was able to communicate with the different mems sensors and I am successf...

NHarb by Associate
  • 1559 Views
  • 2 replies
  • 0 kudos

VL53L1x motion feature enhancement

Hi. I want to use VL53L1x time-of-flight sensors in following scenarios:detect an empty hand and a hand with an item using gesture detection approach;detect the product movement up or down. Have done several tests to understand the dependence between...

KKoma by Associate
  • 822 Views
  • 0 replies
  • 0 kudos

LIS3DH read data not reasonable?

Hi I'm currently implementing a crash detector in our device. And it works quite fine, but I think the received values are not correct. The sensor is on a PCB which is already delivered and should be enabled as a new feature in the future. So they de...

capture by Associate
  • 2060 Views
  • 1 replies
  • 0 kudos

LIS2DH12TR accelerometer sensor

Hi ,I'm trying to read the accelerometer data from the LIS2DH12TR which is connected to CC1310 TI's Controller.In my design I'm using I2C hence i have connected the CS pin to Vdd(3.3V) and SA0 pin to VDD. As per the Data sheet with my case the addres...

LN by Associate II
  • 2858 Views
  • 5 replies
  • 0 kudos

LSM6DSL: FIFO mode pattern and timestamp & temperature

Hi, I am new in Embedded software. I am doing a research and trying to extract the data from the LSM6DSL using FIFO mode. I have set the fifo, gyro, accel's ODR to 833Hz with no decimation factor.No thresholdDisable 3rd and 4th data setEnable roundi...

jb by Associate II
  • 1157 Views
  • 0 replies
  • 0 kudos

My LIS3DH seems broken, and the self test results are weird

Hi, I'm using the LIS3DH to detect body movement, but I'm suspecting that the accelerometer is defective as the samples do not seem reasonable (for example, when testing a single axis and turning it all around, it won't go from 1 to -1 g).I wrote a p...