MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HB post solder correction

Hi, I am using the LPS22HB and noticed it was reading significantly off after installation. The datasheet and applications notes really don't address this and a good way to correct for it. Could you look at enhancing your application notes or techni...

AIS3624DQ Not Functional Unless i2c lines are high.

I am using the STEVAL-MKI158V1 eval board which uses the AIS3624DQ. When I deinit the i2c communication to the device the sca and scl pins go low and the AIS stops outputting interupts. I can confirm the interupt pin triggers when the i2c connection ...

JMari.18 by Associate
  • 2060 Views
  • 4 replies
  • 0 kudos

LIS2DW12 interrupt on stop motion

I'm looking for the best way to send an interrupt on when the LIS2DW12 senses that motion has stopped.Ideally, the LIS2DW12 will be sleeping until it senses that it is moving...like in a car. The LIS2DW12 will only be moving for about 10 to 500m in ...

HReis by Associate
  • 1198 Views
  • 1 replies
  • 0 kudos

[MPU9250][AK8963] Read magnetometer data problem

Hey.I have a small problem with the MPU9250 module, and more specifically AK8963 (Magnetometer). Reading the values ​​measured by the accelerometer and gyro did not cause me major problems and everything works properly. The matter was complicated whe...

MNowa.10 by Associate
  • 3105 Views
  • 1 replies
  • 0 kudos

Resolved! LIS3DH - Error in C-Driver-MEMS

The Standard C platform-independent drivers for MEMS motion and environmental sensorshttps://www.st.com/content/st_com/en/products/embedded-software/mems-and-sensors-software/drivers-for-mems/c-driver-mems.htmlThe LIS3DH Temperature Sensor is connect...

MotionFD and SensorTile compatibility

Hello ST Community,I would like to ask if the (1)SensorTile and/or (2)SensorTile.box are compatible with the MotionFD library?According to the MotionFD user manual, the library uses Accelerometer and Pressure Sensor data to detect a fall, which both ...

DIM by Associate II
  • 1159 Views
  • 1 replies
  • 0 kudos