MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM9DS1 Library

Who knows where can get LSM9DS1 Library for STM32?I ever find the X-CUBE-MEMS Library, but I didn't find LSM9DS1 library. And then, If it can use, but its magnetometer different to X-NUCLEO-IKS01A3of LIS2MDL. How should modify by its library?

Reading HALL Sensors values from HALL interface

Hi dear members, I am trying to understand complete how to drive bldc motor.And I would like to use hall interface in stm32.how can I manage to read commutation using hall sensors which registers I couldn't find it in reference manuel.And also how ca...

Zek_De by Senior
  • 4734 Views
  • 6 replies
  • 0 kudos

STM32CubeProg failed to download FP-AI-SENSING1

Hello,STM32CubeProg outs "Error: failed to download Segment[0]" and failed to download FP-AI-SENSING1(SENSING1.hex).My envs are,SensorTile kit with small cradle.The FP-AI-SENSING1 ver.3.0.0The project is imported from SW4STM32 to STM32CubeIDE ver.1.0...

Yuk117 by Associate III
  • 1884 Views
  • 1 replies
  • 0 kudos

HTS221 and condensation

The HTS221 has an internal heater to "speed up the sensor recovery time in case of condensation".How do I identify a condensation state?How long the heater has to be activated, in order to recover from condensation state (I want to estimate power con...

GShim by Associate II
  • 2303 Views
  • 6 replies
  • 0 kudos

LIS3DH Low-power mode

LIS3DH MEMS digital output motion sensor.Hi every body.I'm using this sensor in 'High-resolution mode'. but after some time (I define timeout = 10 seconds) without detect any motion, put the sensor in 'low-power mode'. if the sensor is moved before t...

LM by Associate II
  • 1215 Views
  • 1 replies
  • 0 kudos