What are the differences and advantages between the LIS2DH12 and LIS2DW12 ?Please let me know if I do want to use this sensor for detection the device is not moving in any directions (NO MOTION) at very low current consumption then which ONE i should...
Please help:I had STSW-MKI109W with STEVAL-MKI196V1Not Recognize the board on Windows 10Device manager shown:What is the driver for my Windows 10Thanks
I want to set up the interrupt for system power off the main MCU, the STM32L4 xx .As soon it is powered on, then starting the timer to turn it off after 2- to- 4 Hours.Please point me how to implement it since I'm still new for STM32L4xx