MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Best controller for a music player?

Hi All, I'm trying to build a MP3 player. So, I need suggestions like which ST controller would be best for me to build a MP3 player. Also, for a head start are there any suitable development boards available, on which I can proceed with the coding p...

SensorTile.box #2: One structure, infinite applications

Have you ever wondered how to build a plug-and-play barometer, or a pedometer, or even a vibration monitoring? This is almost immediate with a SensorTile.box. Once the BLE connection is set-up and the last FW has been downloaded, the Example app scre...

0690X00000ARY5pQAH.png

LIS2DW12/LIS2DTW12 OCR Timing Accuracy

Regarding the LIS2DW12 and LIS2DTW12 devices, there is no published specification on the accuracy of the ADC sampling frequency in the datasheet, nor it's drift against temp and supply voltsage. Without these data the selected ODR is a guess, e.g. 40...

AMoul by Associate II
  • 1401 Views
  • 3 replies
  • 0 kudos

Zero-g values for IIS2DH

I am using IIS2DH accelerometer for vibration analysis. As per the datasheet the Zero-g level for x and y axis is 0 while z axis measures 1g. For my application when the device is resting x and y shows zero but z shows the value which give wrong read...

YMand.4 by Associate
  • 1092 Views
  • 2 replies
  • 0 kudos

LSM6DS3 fifo read via i2c

I have been reading a 780 samples from lsm6ds3 FIFO via i2c (i2c_dev driver from linux) but the read is taking arround ~1.5 to 2 sec. this seems little unusual to me . is there any way to reduce the i2c read time ?.Here is my read function:static int...

thejas by Associate II
  • 1498 Views
  • 2 replies
  • 0 kudos

About the LPS22HH' s temperature compensation

HiWe are testing the LPS22HH on the MKI192V1, and we have got the pressure and the temperature. We also convert the pressure value to the height.We put the LPS22HH in the metal shell, and It is not sealed. We use air guns to heat the shell, and we fi...

User.120 by Associate II
  • 1571 Views
  • 2 replies
  • 0 kudos