cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to use the VL53L0Cx in my design. Is there a drawback to use it at 3.3V (instead of 2.8V as recommended) ? Also the spec is not clear about if the GPIO1 interrupt output is active low or high (I'm guessing active low...).

JoBrodeur
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

​3.3 volts is perfectly fine. Well within the range of the device. Not an issue. Please insure you don't exceed the max range. That would be bad.

The interrupt is active low by default, but there is an API to change that.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.