cancel
Showing results for 
Search instead for 
Did you mean: 

tranking cricket bat swing. with motion fx library.

kasi viswanadh
Associate II

I want to track the swing of cricket-bat using mems sensors. i'm running Motion FX library at 100hz and 200hz. motion fx library is failing some times to track the orientation if the swing speed is more . can I run MotionFx sensorfusion library at 300 hZ? can I use FIFO data and pass more number of input data to compute orientation without increasing the sensorfusion rate?  

Thanks in advance.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0