MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Convert I3G4250D gyro raw output to understandable values

Hello STM32 community,I'm relatively new to STM32 development and I'm currently working with the I3G4250D Gyro Sensor on the STM32F411e-Discovery board. I've been using the stm32f411e_discovery_gyroscope.c file (BSP Drivers) provided by STM32Cube to ...

Kushal_Es by Associate II
  • 1274 Views
  • 1 replies
  • 0 kudos

i3g4250d - Getting same XYZAngRate value on every read

Hi,I have a i3g4250d sensor chip on our custom board with STM32G474 MCU.I have used the below driver github.com STMicroelectronics stm32-i3g4250dfor reading the sensor chip registers through SPI interfaceI am able to read "WHO_AM_I_ADDR" register wi...

PKupp.1 by Associate
  • 2765 Views
  • 4 replies
  • 0 kudos

Resolved! LIS2DW12 INT1 Pin Goes High After Reinitialization

Hi,I'm working with the LIS2DW12 accelerometer in a low-power IoT application. The sensor is configured to wake the MCU via an interrupt on INT1, connected through a monostable multivibrator (Schmit trigger IC). The setup is designed so that a rising...

Resolved! STEVAL-IDP005V1-GUI does not connect

Hi.i am having a STEVAL-IDP005V1, STEVAL-UKI001V1, 10-pin-IDP005V1 Cable, M12female connector.i am referring this document ( https://www.st.com/resource/en/product_presentation/steval-bfa001v1b_quick_start_guide.pdf ) i am not able to connect the boa...

Unresponsive LPS22HHTR

Hi all, I have installed the LPS22HHTR on my custom circuit to communicate with a STM32F4x via I2C. I have pulled up the SCL (pin 2), SDA (pin 4), SA0 (pin 5), and CS (pin 6) lines to 3.3V via 4.7k resistors, grounded the two ground pins (8 and 9) an...

boof by Associate
  • 2475 Views
  • 2 replies
  • 1 kudos

STEVAL-IDP005V1-GUI does not connect

HiI am trying to run the STEVAL-IDP005V1-GUI.Current setup:STEVAL-IDP005V1-GUI - > STEVAL-IDP004V1->STEVAL-IDP005V1:I am unable to connect to the IDP004V1 dev kit from the GUI, the comms just gives an error suggesting to restart the GUI. I have tried...

Tvan .5 by Associate
  • 2103 Views
  • 5 replies
  • 1 kudos

Nucleo-U385RG-Q with LPS22HH using I2C times out

Hi, I am using STM32CubeMX to configure STM32CubeIDE project. I have Nucleo-U385RG-Q with MEMS X-Nucleo-IKS01A3. I am trying to read pressure sensor LPS22HH. According the X-Nucleo documentation the I2C default addresses for LPS22HH are: BA and B8. B...

suiunbek by Associate II
  • 1358 Views
  • 2 replies
  • 0 kudos

LIS2DE12TR accelerometer input capacitor query

Has anyone tested the LIS2DE12TR accelerometer using lower input capacitance? I am interested in trying it out and possibly using it in an intrinsically safe design and the recommended 10uF capacitor is a deal breaker. Alternatively, does ST have a s...

TJL by Associate
  • 609 Views
  • 0 replies
  • 0 kudos

lsm6dsv with lis2mdl sensor hub

HelloI would like to get the lis2mdl magnetometer data using the lsm6dsv second i2c line using the sensor hub.so far I get the accelerometer and gyroscope data via SPI and I want to add the magnetometer data.The code I have to configure the sensor hu...

Eddess by Associate II
  • 1141 Views
  • 1 replies
  • 0 kudos