2023-03-02 4:38 AM
Hi,
I have a i3g4250d sensor chip on our custom board with STM32G474 MCU.
I have used the below driver
github.com STMicroelectronics stm32-i3g4250d
for reading the sensor chip registers through SPI interface
I am able to read "WHO_AM_I_ADDR" register without any issue that confirms my SPI interface is fine and communicating with sensor chip
but
when I read XYZ values I always get the same value irrespective of sensor position.
My sensor init configurations are
CTRL_REG1 = 0x3F
CTRL_REG4 = 0x10
When I read the STATUS_REG, the first read shows 0xFF and consecutive reads always shows 0x00
What could be the problem.
PS: I have a Accelero meter sensor chip lsm303agr on the same board configured with I2C interface which is working properly.
Thank You
Prabhu M K
2023-03-03 6:02 AM
Hi Prabhu M K @PKupp.1 ,
do you see any particular issue in the SPI oscilloscope patterns? Are you using SPI 4 wires?
-Eleon
2023-03-07 5:02 AM
Hi Eleon,
I got another board assembled.
In this i get an different issue. I get random XYZ values even though the board is stationery.
STATUS_REG reads 0xFF and 0xB3 on every alternative reads.
Below my SPI configuration, I am using 4 wire.
SPI Clock speed 5.3125 Mhz
/* USER CODE BEGIN SPI1_Init 1 */
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
/* USER CODE END SPI1_Init 1 */
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 7;
hspi1.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE;
hspi1.Init.NSSPMode = SPI_NSS_PULSE_DISABLE;Regards,
Prabhu M K
2024-02-15 4:07 AM
Hi Prabhu M K @PKupp.1 ,
Have you got the answer of the above problem, because i am also facing the same issue with STM32F411VET6 and sensor is the same I3G4250D.
2025-05-07 5:17 AM - last edited on 2025-05-07 5:34 AM by Andrew Neil