MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to connect more LSM303AH on one SPI BUS?

We are affraid when one device has CS signal down, other devices will be set to I2C there can be conflict on the SPI BUS. Is it possible connect more devices as eclosed schematic?

Using X-CUBE-MEMS1 for lsm9ds1

Hi, I want to use -CUBE-MEMS1 for lsm9ds1. By default the applications code uses LSM303AGR . Could any one give me some hints what changes I need to do for porting ECompas application for lsm9ds1. I have already ported the driver accelerometer, gyro...

Resolved! LIS2DH false positives in detection of clicks

Hello all,I am having an issue with single-click detection. I am getting false click detections at certain threshold values. I found this out yesterday when I had an MCU register lots of clicks repeatedly, but the device was not being shaken.To test,...

(LSM6DSL) how to get total G-Force

(Because I am not good at English, I used Google Translator.)​I'm using the LSM6DSL sensor now. I think that with this sensor still, the total gravity acceleration should be 1G, or 9.8.( Total - G - Force = SQRT(x^2 + y^2 + z^2 ) ) ​However, as the s...

Edoyo.1 by Associate
  • 1265 Views
  • 1 replies
  • 0 kudos

How to get MEMS board working with CubeMX?

Hi,I have just started my journey with STM products. I have STM32WB board with MEMS IKS01A3 extension board. I am trying to configure project using CubeMX software to generate code. I have created new project and added board extension IKS01A3, tunred...

LZure.old by Associate II
  • 1265 Views
  • 1 replies
  • 0 kudos

Hi, i need some help writing code of Heart Beat sensor max0100 I connected it to STM32L476 Discovery controller and activated the I2C pins in the STCUBE32IDE program. I dont know how to configure the MAX30100 in order to work with the controller

max 30100DataSheet - https://datasheets.maximintegrated.com/en/ds/MAX30100.pdfvideo explained the code for temprature sensor https://www.digikey.co.il/he/maker/projects/getting-started-with-stm32-i2c-example/ba8c2bfef2024654b5dd10012425fa23the contro...

YBuch.1 by Associate III
  • 2245 Views
  • 4 replies
  • 0 kudos

LIS2DH taking more than 100 uA

We are using LIS2DH in our board for production. Among 1000 boards, about 50 boards were drawing much more power because of LIS2DH (the IC is functional - we are getting the accelerometer data). Once we remove the IC from the board, current dropped f...

PK.1 by Associate II
  • 2705 Views
  • 7 replies
  • 0 kudos

Resolved! Cannot power down LIS3MDL

HI all,I cannot set sensor to power down mode.When i send command 0x03 to register CTRL_REG3, Current consumption is 100uA, i use stm8l151g6 (turn off hardware LIS3MDL current consumption is 1uA).

NPhuc by Associate II
  • 1002 Views
  • 1 replies
  • 0 kudos