Skip to main content
Andrew Neil
Super User
Aug 12, 2019 5:17 PM UTC
Question

Unicleo - Comms protocol? Source code?

Is the comms protocol between the Unicleo GUI PC application and the Nucleo board documented anywhere?

If so, where?

The Unicleo GUI is touted as part of the "Open Development Environment", but I can't see any source code anywhere.

Is it published?

If so, where?

    This topic has been closed for replies.

    4 replies

    Eleon BORLINI
    ST Employee
    Aug 13, 2019 8:28 AM UTC

    ​Hi @Andrew Neil​ , unfortunately the full source code of the Unicleo-GUI is not available. However, if your target is to display a data in Unicleo-GUI, you can use Datalog Custom mode. The example of the Datalog Custom FW is available in X-CUBE-MEMS-XT1 and it is described in UM2142. This package library, which directly interfaces with the X-NUCLEO-IKS01Ax HW family, is open. Regards

    Andrew Neil
    Super User
    Aug 13, 2019 10:08 AM UTC

    OK, thanks.

    Yes, it's sending the data to Unicleo that's the main interest - hence a specification of the protocol.

    I have seen that the X-CUBE-MEMS1 package contains a "DataLogExtended" application - is that the same thing?

    In that, the readme.txt fir the STM32L476RG-Nucleo example for IKS01A3 says,

     - WARNING: this sample application is only compatible with the Sensors_DataLog PC utility version 1.4.0 or higher;
     it does not work with previous versions of the Sensors_DataLog application.

    Is "the Sensors_DataLog PC utility version 1.4.0 or higher" the same thing as the "Unicleo GUI" (presumably just before that name was invented) ?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    ST Employee
    Aug 15, 2019 7:29 AM UTC

    Hi @Andrew Neil​ 

    the low level protocol is described in attached file.

    It is implemented in serial_protocol.c you can reuse this file if you want.

    For the data stream content please check the DataLogCustom and the UM2142, this mode is the only way how you can send custom data to Unicleo-GUI.