Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
data[0]=0B10001111; data[1]=0B00000000;data[3]=0B00000000; //this is not needed but i get the default answer here SPI.beginTransaction(SPISettings(100000, MSBFIRST, SPI_MODE3)); digitalWrite(10, LOW); delay(10); for (size_t i = 0; i < datale...
Hi , is there any sample code for interfacing lis3dsh accelermeter sensor to stm32f103rb evaluation Board.Regards,manjunath
Hello,I am trying to setup INT2 pin on LIS3DH. I can successfully setup INT1 without any issues and confirm an interrupt has fired with INT1_SRC (0x31). I am trying to setup INT2 pin the same and confirm when it fires by reading INT2_SRC (0x35) but c...
Within a research project we are evaluating the IIS3DWB for measuring vibrations in hydraulic forging hammers for predictive maintenance.The current application requires that two IIS3DWB sensors (which are connected to the same microcontroller) are s...
In fact, I want to read the real time data MMA8452 working with STM32L476RG, I need to know if there is a C library that I can use in this case, if not, how i can develop a C library for this accelerometer giving the technical sheet.
hi st: I am using lis2dh, driven by spi. Initially set to fifo mode, 25hz. When the power is turned on for the first time, I can read that there is data in the fifo, and the data are normal. When I reset the mcu and initialize the sensor again, th...
Is there a Problem when the Sensor is sampling and doing a i2c communication(reading the FIFO) in parallel?I saw that, that the FIFO gets shifted(or data is overwritten) a few times during collecting data.Can someone help me please?Best Regards,Chris...
It is stated that the 220nF capacitor should have a ESR smaller than 200mOHm. At what frequency is this rated? not sure what frequency the LSM is switching this capacitor. I had a look at the EVAL MKI72V1, but that one has an error in the BOM. Any su...