MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is modulus of acceleration?

In Design Tip DT0106, is it mentioned that:Another technique which can be of help in controlling the integration error is known as Zero-Velocity-Update (ZVU): when the modulus of the acceleration is 1g and the output of the gyroscope is near 0, then ...

NLe.1 by Associate
  • 2053 Views
  • 2 replies
  • 0 kudos

Transferring PDM_OUT from MP45DT02 to CS43L22

I want to access PDM_OUT data from the MP45DT02 and output this on the CS43L22. For this I want to use the I2S protocol but I have difficulties connecting the MP45DT02 to the I2S mode and using the HAL_I2S_Receive function. How do you initialize the ...

JtotheF by Associate
  • 1079 Views
  • 1 replies
  • 0 kudos

VL53L0X CALIBRATION

Hello, I am writing this message to you because I need help, if it is possible I would be grateful to you .. Ok, I am working on a project in which we will use the VL53L0X as a sensor in an access control device , we will use it as a proximity sensor...

MSAMB.1 by Associate III
  • 872 Views
  • 0 replies
  • 0 kudos

VL53L0X Offset Calibration Procedure Examples?

I'm using an array of VL53L0X for a robotics application, and I'm struggling with the problem of offset calibration. I have looked through the API, but I get lost pretty quickly. Can you point me at any working tutorials and/or examples showing how...

FPayn.1 by Associate III
  • 826 Views
  • 1 replies
  • 0 kudos

SensorTile.Box hangs when logging acceleration data to SD card

I am trying to log acceleration values, time and date over a longer period of time. (8 hours)After an undefined time (often after about 1h) the green LED will no longer flash. If the SensorTile.box is supplied by a power supply, you can see that the ...

KBerg.1 by Associate II
  • 1906 Views
  • 4 replies
  • 0 kudos