cancel
Showing results for 
Search instead for 
Did you mean: 

ERROR MESSAGE

MSAMB.1
Associate III

HI everyone,

I have this error message when I compile my main program with eclipse ... I'm using a P Nucleo 53L0A1 .. someone can tell me what's happening because I really don't understand

error message =>

Open On-Chip Debugger 0.10.0+dev-00021-g524e8c8 (2019-04-12-08:48)

Licensed under GNU GPL v2

For bug reports, read

http://openocd.org/doc/doxygen/bugs.html

C:/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.debug_2.5.0.201904120827/resources/openocd/scripts/st_board/nucleo_l476rg.cfg:15: Error: Can't find target/stm32l4.cfg

in procedure 'script' 

at file "embedded:startup.tcl", line 60

at file "C:/Ac6/SystemWorkbench/plugins/fr.ac6.mcu.debug_2.5.0.201904120827/resources/openocd/scripts/st_board/nucleo_l476rg.cfg", line 15

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Julien NGUYEN
ST Employee

​Hello,

I would use the example code provided in X-CUBE-53L0A1 to check if your AC6 IDE is working and base on the example code structure to develop your own code.

Thanks,

Julien


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.