MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LSM6DSO Migration from LSM6DSM

Hi Everyone,I'm currently migrating from LSM6DSM to LSM6DSO in my application and facing some issues with accelerometer accuracy in stable conditions.System Overview:MCU: STM32L4Sensor Interface: SPI (3-wire)Purpose: Reading raw accelerometer and gyr...

rshar21_0-1752843355517.png rshar21_1-1752843410485.png
rshar.21 by Associate II
  • 652 Views
  • 6 replies
  • 0 kudos

MEMS Studio: Failed to parse log file on IR Algorithms Tuning

I'm using a STEVAL-MKI109D with the IR sensor STHS34PF80 and I need to fine tune it to detect objects with low IR emissivity, but everytime I want to load the log file into the IR Algorithm Tuning, the same error appears "Failed to parse log file". I...

RVM by Associate II
  • 287 Views
  • 4 replies
  • 0 kudos

The power consumption of LIS2MDL in power-down mode

Hi,everyone.I measured the power consumption of LIS2MDLTR on the same board in power-down mode.and found that the LIS2MDL chip on STEVAL-MKI217V1(from mouser) consumes less power than the LIS2MDL purchased separately from mouser.We have some question...

young by Associate
  • 146 Views
  • 3 replies
  • 0 kudos

Resolved! sths34pf80 + lens

Hi!We are working on product that needs to count people on the range of 3-4 meters. We designed dev.board for sths34pf80 and tetsted it with UNICO-GUI. The max range that we are getting is around two meters and therefore it looks that we need to use ...

apallo_0-1693465987293.png
apallo by Associate
  • 3422 Views
  • 6 replies
  • 0 kudos

Resolved! STEVAL-MKI109D Software-Adjustable Power Circuitry

Hi,I'm trying to write custom firmware for the MKI109D. I am currently using an MKI251A adapter board with it for evaluation. How do I set VDD_DUT and VDDIO_DUT to 3.3V on the MKI109D board without using MEMS Studio?   

mki109d_power_supply.png