MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Suggest me an accelerometer sensor for speed calculation of moving vehicle.Dynamic values of an accelerometer.

I want to use an accelerometer to calculate the speed of a moving vehicle. For this i need a accelerometer which should give _ve values(2's complement) in Deceleration and +ve values in (2's complement) in acceleration. It should have 2g range with 1...

NMale.1 by Associate III
  • 1369 Views
  • 1 replies
  • 0 kudos

Resolved! SAMSUNG Galaxy j5 accelerometer

HiIm using samsung galaxy j5 accelerometer for a research work about automobile acceleration and deceleration. As you know samsung electronics uses stm mems sensors on its smartphones. In case of galaxy j5, based on some papers, the accelerometer nam...

AAyat.1 by Associate
  • 2045 Views
  • 2 replies
  • 0 kudos

Resolved! Accelerometer circuit LIS2DE12 & Ultrasonic welding.

We are developing a new product with the LIS2DE12 and are planning to use Ultrasonic welding during assembly of the ABS plastic enclosure. The welding machine will hammer on the enclosure with a frequency of 20KHz, with an amplitude of 20umeter and a...

RLund.2 by Associate
  • 1415 Views
  • 1 replies
  • 0 kudos

Resolved! What type of filter is it?

In application note said that "The accelerometer sampling chain is represented by a cascade of three main blocks: an ADC converter, a digital low-pass filter (LPF1) and the composite group of digital filters". I want to know what type of filter is LP...

VSavenia by Associate III
  • 2881 Views
  • 4 replies
  • 1 kudos

Resolved! Accuracy and variability of LIS2DE12 output data rate

I'm attempting to use LIS2DE12 at it's maximum ODR (Nominally 5376 Hz) to accurately measure the vibration frequency of a piece of equipment.I have discovered that the ODR of my sample accelerometers is not the same. The first one that I tested was a...

MMora.6 by Associate II
  • 1597 Views
  • 2 replies
  • 0 kudos