MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LSM6DS33 WAKE_UP_SRC register not providing correct status data.

I have Pololu breakout containing a LSM6DS33 connected to a ESP32 module via I2C. INT1 is connected to GPIO15. I am driving Activity and Wake Up to INT1. The ESP32 picks up the interrupts reliably. I would like to know whether the LSM6DS33 is active ...

BZaai.1 by Associate II
  • 2037 Views
  • 5 replies
  • 0 kudos

Problem installing X-Cube-Mems1

Hi, I am trying to install mems1 with cubemx and cant get it to complete. The file downloads and the "installer" in CUBEMX appears to crash. The screen stops like in the attached picture. I have tried rebooting the machine (PC) and left it over night...

0690X00000AABGHQA5.jpg
FSTKMARO by Associate II
  • 1289 Views
  • 1 replies
  • 0 kudos

IIS3DHH accelerometer temperature drift

The datasheet reports an offset drift TCOff of max. 0,4mg/°C. We made temperature tests with 3 samples and found the offset drift beeing 0,17 ... 0,58 mg/°C so higher than allowed. Does this meet your expectations? Can you share your measurements? T...

GBra by Associate II
  • 7251 Views
  • 10 replies
  • 0 kudos

How to introduce IIS3DWB and IISDH

Hello, I'm working with the STEVAL-STWINKIT and I need to use some accelerometers like IIS3DWB and IISDH. I try to add the software packs using the .ioc (software packs -> select components -> board parts -> X CUBE MEMS1) but they never appear. I don...

0693W000005AKYXQA4.png
AGasc.2 by Associate II
  • 2950 Views
  • 5 replies
  • 0 kudos

I would like to know what device and model to use for an wireless application where I will have 1 stm32 as a master micro controller waiting to receive data and transmit data(two-way communication) from 5 slave stm32 microcontrollers.

The Master stm32 controller need to send talk with the particular slave in order to turn a LED . By using switch,i will turn off the led in the slave controller .The slave has to sent state of led to master controller .There will be cases when maybe ...

Rmajj.1 by Associate II
  • 2907 Views
  • 5 replies
  • 1 kudos

Resolved! Raw data from lsm6dsox

Hello,In my test board, data from accelerometer and magnetometer are stable.But gyro data has many spikes even though it is put in desk and not moving.Do you have any idea for what cause this and how to fix it?lsm6dsox and lis3mdl are used for test.

0693W000005CYLqQAO.png
JPARK.2 by Associate II
  • 2231 Views
  • 3 replies
  • 0 kudos

IIS2DLPCTR: Why are Out_X,Y,Z values are constantly changing?

I got my PCB from the fab today. I am running a test program based on the code in https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/iis2dlpc_STdC/example/iis2dlpc_read_data_polling.cSince the Sensor-PCB is on my desk with no...

VJaha.1 by Associate II
  • 1660 Views
  • 2 replies
  • 0 kudos