Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Greetings - what are the recommended maximum current ratings for the INT pin in either Push-Pull or Open-Drain? And FWIW, I was really surprised NOT to find this published in the datasheet...TIA,-Terry
Hi,I would like to confirm if setting LSM6DSO ODR to 6.66KHz and LPF2 to ODR/10 (resulting to 666Hz bandwidth), then setting a FIFO decimation factor of 8 (resulting to 833hz FIFO ODR) will work in preventing aliasing for signals above 417Hz? We have...
Hi All,I am currently working on a health tracker/monitor project that utilizes the LSM6DSOX sensor, interfaced with the nRF5340 platform and running Zephyr. So far, I have successfully implemented tilt and tap detection features.As the next step in ...
Hello, community! I recently purchased the SensorTile Box Pro to conduct various educational experiments. It connects via Bluetooth to my phone, but when I try to connect it to my laptop using the MEMS STUDIO application, it does not work via either ...
Hey everyone, I’m working on a low-power motion tracking project using an LSM6DSL IMU to capture 3D acceleration and gyroscope data. This sensor is interesting because it has an "Always-On" mode, which is supposed to keep motion detection running wit...
Hi,I am really new to this sensor and I was able to get the polling mode working.I am planning for full 6.6k odr rate and FIFO samples can be 256 when INT1 should be triggered or whenever possible so I can use FIFO .I am really confused with the orde...
Posted on June 09, 2017 at 16:37Hello everyone,I Would like read the lsm6dsl data by interrupt using the pin int1 on the sensor.I configured the accelerometer ODR to 104 HzAnd i set up registers as follow : - Control_3C (0x12) = 64 (Data updated on...
Hi,I want connect my SensorTile box with my Raspberry pi. For this, I use example_ble_1.py, but every time when i try to connect the devices then one of the given errors occur:guest@raspberrypi:~ $ sudo python3 example_ble_1.py##################BlueS...
I have a problem with identifying the sensor type from the marking on the housing. One is LSM6DSO32XTR and the other is ASM330LHHXTR. Unfortunately they came in a bag without a description on the label. One is marked T3 [QR code] 233 and the other LC...