MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! LIS2DW12 MEMS sensor scales

Hello everyone, I hope you are well and in good health.I am currently working on an academic project "Parking Barrier Command". For this application, I am going to use the MEMS sensor LIS2DW12.Checking the sonor specifications, it shows me that it ha...

WBen .2 by Associate II
  • 1247 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DW12 adding to interrupt2

Hello @Eleon BORLINI​  ,l want to add functionality to interrupt 2, I want that in addition to the full fifo we have. how can i do it?

Msaga.1 by Associate II
  • 2428 Views
  • 4 replies
  • 0 kudos

How to get rid of audio spike of MP34DT06JTR in STEVAL-BCNKT01V1. and and the frequency response does not follow the specification. + Power issue

Hi,I am working with STEVAL-BCNKT01V1 (Bluecoin board) with the sample project FP-SNS-ALLMEMS1 and BlueMS for android (with default configuration.) I found that there are many spikes in the mic signal occurring every 20-70ms. To make sure the hardwar...

TOuyp.1 by Associate
  • 1774 Views
  • 2 replies
  • 0 kudos

Abnormal output value from ASM330LHH gyroscope. Gygroscopoe no feedback when I move, vibrate or knock the product, but the output data have noise (may show the sensor is not damaged?)

I got a gyroscope problem when i use asm330lhh to develop a new product, and need your help.Gyroscope of ASM330LHH got abnormal output value, detail as follow.1) gyroscope zero offset is much bigger than usual.2) gyroscope noise is much bigger than u...

0693W00000Bcjl2QAB.jpg
Teni CC by Associate
  • 1580 Views
  • 2 replies
  • 0 kudos

Resolved! MTBF

Dear support I need the reliability data (FIT or MTBF) for LSM6DS33 and for LPS25HB

Rcana.1 by Associate
  • 2448 Views
  • 2 replies
  • 0 kudos

Resolved! How do I calculate the gyroscope sensitivity?

Hello,I'm integrating the LSM6DSO32 into an MCU project and I'm using the example drivers from CubeMx.The problem is that I don't understand how the gyroscope sensitivity is calulated into the drivers. The constants for the sensitivities at the vario...

DGiov.1 by Associate III
  • 6077 Views
  • 8 replies
  • 0 kudos

ISM330DLC device ID

Hi,I have made a module using ISM330DLC IC. I made the schematic by taking reference from STEVAL-IDP005V1 schematic. PFA, both the schematics.Now, I am using Nucleo -F44RE board to interface this module using SPI.Also, using the libraries for the ISM...

RJain.1 by Associate III
  • 4228 Views
  • 6 replies
  • 0 kudos

I am trying to deploy dsh-predmnt to my personal aws account but serverless is throwing a lot of errors. I followed the PDF document "How to deploy DSH-PREDMNT in proprietary AWS account" . Is there a more detailed instruction on deploying to AWS??

PS C:\pm\predictive_maintenance_fe\serverless>node --versionv14.16.1PS C:\pm\predictive_maintenance_fe\serverless>npm --version7.11.1PS C:\pm\predictive_maintenance_fe\serverless>npm install   up to date, audited 190 packages in 2s   6 packages are l...

VChak.1 by Associate II
  • 4616 Views
  • 8 replies
  • 1 kudos

Resolved! ST BLE Sensor App and Dashboard - Offline.

I've the STEVAL-STWINKT1B,I've flashed ,\STMicro\SW\en.fp-sns-datalog1\STM32CubeFunctionPack_DATALOG1_V1.1.0\Projects\STM32L4R9ZI-STWIN\Applications\HSDatalog\Binary/HSDatalog.binBut I do not able to read the sensor data.I do not access the environme...

LK N.1 by Associate II
  • 3642 Views
  • 11 replies
  • 0 kudos