MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L1X Long-distance Ranging sensor: I have planned to integrate this sensor into my board. How is the I/O supply of 1.8V (standard mode) generated internally from the AVDD supply? Will there be any issue when I provide 2.9V (or) 3.3V supply to AVDD?

On my board, I have two supply options within the permissible range of this sensor (2.6~3.5V) i.e. 2.9V & 3.3V. Will there be any switching noise coupling to the power supply due to the ranging operation of the sensor? Are there any recommendations t...

MM.11 by Associate
  • 1129 Views
  • 1 replies
  • 1 kudos

Resolved! Why does ST VL53L0X library always return RangeStatus non-zero

We are using the VL53L0X sensors in their default configuration supplied out of the factory. We run VL53L0X_DataInit() on the sensors and then every 100ms call VL53L0X_PerformSingleRangingMeasurement(Device, &measure). Upon return, we check measure.R...

Resolved! How to use VL53L0X_CHECKENABLE_RANGE_IGNORE_THRESHOLD

We tried to use VL53L0X_CHECKENABLE_RANGE_IGNORE_THRESHOLD.But not found any effect on measurement reading.If you share some input for way to use VL53L0X_CHECKENABLE_RANGE_IGNORE_THRESHOLD, then it will be very useful.

YGude.1 by Associate II
  • 1296 Views
  • 1 replies
  • 0 kudos

Resolved! VL6180V1 for measuring the level of water - Will it give me the height of water or distance of water from sensor

Hello. I would like to measure the level of water in a closed container.I have chosen VL6180V1 for the same since it has an 850 nm light source which won't be absorbed by water.I have referred this article for it:https://community.st.com/s/question/0...