cancel
Showing results for 
Search instead for 
Did you mean: 

I have calculated the threshold value by setting the offset voltage of 3.3V and the the reference voltage of 5v for the 12 bit adc of 1024 states. I calculated 1024/5=x/3.3v which equals approximately 716.8.

SANAN.1
Associate II

Can I know how can I set this value in terms of Force or Pressure?

Like the representation of this value in terms of force or pressure??

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Eleon BORLINI
ST Employee

Hi @SANAN.1​ ,

I believe you should multiply the voltage value for the sensitivity (usually expressed in Pa/V or in N/V for an analogic pressure or force sensor), that is usually reported in the sensor datasheet.

By the way, which ST sensor (part number) are you using?

-Eleon

I am using Piezo Sensor to get the Hpatic Feedback

Haptic*