MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L1x People Count by using Interrupt method

Dear Team,We are using VL53l1X in our application to detect people leaving and entry, we got 5 vl53l1x breakout boards from one of my distributors for prototyping.People count programming working without any issues when using it in polling/continuous...

MMari.2 by Associate
  • 1620 Views
  • 1 replies
  • 0 kudos

LSM6DSO pedometer interrupt setting

Hello,I am using LSM6DSO sensor to do a pedometer. I use the official interrupt signal to control the step update like the following sentence.int1_route.emb_func_int1.int1_step_detector = PROPERTY_ENABLE;But I found the interrupt signal always has so...

JXiao.1 by Associate II
  • 1675 Views
  • 2 replies
  • 0 kudos

Resolved! Compatibility between LSM6DSL vs LSM6DS3

Hi Sir,We have used the LSM6DS3 part in our application boards. Now the distributor mentioned LSM6DS3 part ha end of life and New part is LSM6DSL.Please confirm this new LSM6DSL part is pin to pin and firmware side compatible with the LSM6DS3 part. ...

APK.1 by Associate II
  • 4410 Views
  • 5 replies
  • 0 kudos

Where can I find STEVAL-STLCS01V1 's external layout?

Hello,I would like to include this board on a custom design but I was unable to find it's pads, connectors layout.There's nothing in the datasheet and only gerbers are available... :(Where can I find this information?ThanksJulien

JulienD by Senior
  • 1042 Views
  • 1 replies
  • 0 kudos

lis2ds12 Bypass to FIFO/Stream example

My test:I want to set up the FIFO for bypass->stream, and then just move (shouldn't have to be a violent shake) the PCB that has the lis2ds12 on it and see the FIFO have data. I'm only able to detect violent shaking... could you please advise / sugge...

ATemp.1 by Associate II
  • 1323 Views
  • 1 replies
  • 0 kudos

Resolved! LSM6DS33 -> Bulk read FIFO

Hello,I am using the FIFO to read the gyroscope and accelerometer data from the LSM6DS33 using a Raspberry Pi. It is connected over I2C at a frequency of 400kHz. Currently it takes between 4-7 seconds of constant reading to empty out the FIFO and by ...

MKama.2 by Associate
  • 1334 Views
  • 1 replies
  • 0 kudos

Resolved! LSM9DS1 FIFO usage

Hello, I tried to use FIFO in way to count data ready . My idea to count sample and if it is a 32 sample in FIFO I read all at once. As far I understand, according by datasheet "Accelerometer and gyroscope multiple reads (burst)" Page 21Data stores ...

Zaren by Associate
  • 1366 Views
  • 1 replies
  • 0 kudos