TWade.1
Associate II
since
2021-07-27
2023-06-14
User statistics
4
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About TWade.1
Options
Report User
User Activity
Posts
Replies
Just wondering are there any examples of how speed could be measured using LSM6DSOX? Or is this even possible using Unico GUI? I know speed = distance/time so technically if you can measure distance and time using LSM6DSOX speed can be inferred? Thanks
2021-10-06
Hi, Using LSM6DSOX and when creating the the ucf files using Unico I would like to be able to decode them. This documentation is available for FSM but will it be available for the ucf files?
2021-08-31
Re: Hi, Using LSM6DSOX and when creating the the ucf files using Unico I would like to be able to decode them. This documentation is available for FSM but will it be available for the ucf files?
2021-09-02
Hi Eleon,Thanks for your reply, I have read those posts but I needed more documentation on the ucf files and registers. Are ST going to document it like the FSM?Thanks Tristan
Re: Unico UCF file format
2021-08-31
Did anyone ever find out an answer to the decoding of the ucf file? Thanks