MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! consume very high current in lsm6dsox

Hi team,we have configured accelerometer normal mode in the sensorBelow configuration - Accelerometer normal modePower mode - Normal modeG-Range - 16 gODR208HZ CTRL8_XL (0x00) CTRL6_C (0x10) CTRL1_XL (0x54)104 HZ ...

0693W00000F9wNBQAZ.jpg
Sprem.1 by Associate III
  • 2106 Views
  • 3 replies
  • 0 kudos

Resolved! If you could pass your knowledge onto a dev starting their vibration project how would you recommend them to start?

I have spent some time on the forums and can see that there are many options for projects depending on the requirements of the user. I am looking to hear people's opinions on a suitable setup as an introduction to the field. I am a firm believer in w...

HADWLL by Associate
  • 1795 Views
  • 3 replies
  • 0 kudos

Resolved! Is it possible to dinamically change the threshold for the FSM?

Hello,I'm working on a ultra low power application using the LSM6DSO32X. The goal is to have a device that reacts (with a short radio message) when its orientation relative to gravity changes. For this I wish to use as much as possible the FSM and th...

DGiov.1 by Associate III
  • 2100 Views
  • 3 replies
  • 0 kudos

Resolved! Question about LSM6DS3h : why Accel Z value OUTZ_L_XL (2Ch) & (2D) become negative when module acceleration downward but not upside down.

I am using this chip to get the X & Y angle of the unit. First read outOUTX_L_XL (28h) & 29hOUTY_L_XL (2Ah) & 2BhOUTZ_L_XL (2Ch) &2Dhand calculate Roll and Pitch.  The angles works good in normal / slow moving or stable condition. Also need to det...

MLy by Associate II
  • 3090 Views
  • 6 replies
  • 0 kudos

Resolved! On the STWIN SensorTile Wireless Industrial Node, the standard en.fp-sns-datalog1_v1.2.0 firmware behaves differently if using the binary, rather than compiling the code in the STM32Cube IDE.

When I compile the code in the IDE and run it (with the acquisition json file set to activate for 5s, then idle for 10s, and repeat) It activates correctly the first time. However, when coming out of idle the second time, it produces an SD card erro...

0693W00000DmSBZQA3.png
LWeir.775 by Associate II
  • 1631 Views
  • 2 replies
  • 0 kudos

LSM6DSM factory reset

I have been working with this sensor for a while. It started to give weird errors such as reading all zeros on all axis. Then sometimes it would initialize but read values like 4, 0, 4 and such. Which is impossible in a static position. I have tried ...

FBoth.1 by Associate III
  • 3176 Views
  • 5 replies
  • 0 kudos