MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Shelf life of pads on the underside of LIS2DH12TR?

Hi,Recently we bought & recived components (MPN LIS2DH12TR) from distributor (Mxxxxx) are over two years old date code, which exceeds the threshold for our internal testing policy.As you know, there's a potential risk of pad oxidation affecting solde...

Resolved! iis2iclx how to read fifo

I want to read acc data by fifo, but int1 can't work. I think there might be something wrong with my setup, but I can't figure out where the problem lies. This is my code. /* Wait sensor boot time */ platform_delay(BOOT_TIME); /* Check device ID ...

Alpha_Lee by Associate III
  • 940 Views
  • 1 replies
  • 0 kudos

Can i measure distance (1mm) using LIS3MDL?

Hello,I am developing a dynamometer to measure the load placed upon it. To do this, I have designed a spring so that a 1 kg load compresses it by 1 mm. Therefore, I need a sensor capable of detecting the spring's displacement with 1 mm precision.My q...

WhatsApp Image 2025-09-22 at 12.30.25.jpeg

Resolved! How to find the euler angles Yaw,pitch,roll in lsm6dso?

Hi,We are using the LSM6DSO in our project to find the euler angles.we are new to this motionfx in stm32. please tell us from where we have to start to find the euler angles.Do we need to add any of the files in the stm32?please tell us from the begi...

TejasK by Associate III
  • 956 Views
  • 2 replies
  • 0 kudos

Resolved! ODR_XL[3:0] operation of ASM330LHH

We sincerely appreciate your continued support. We have been able to resolve many questions.In the CTRL1_XL register of the ASM330LHH, when setting ODR_XL[3:0] from 0000 (OFF) to 0011 (52Hz) and then to 1001 (3333Hz), does ODR_XL[3:0] need to be set ...

ggob by Associate III
  • 617 Views
  • 1 replies
  • 0 kudos