MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I want to use two wake up inrterrupts at the same time. Thresholds and duration will be different. I cannot use it at the same time because I changed the register value while doing the settings.

I want to use wake up interrupt for two different thresholds at the same time,for example I want to give wake up threshold 1g for interrupt 1, I want to give 500 mg for interrupt 2. And duration will be different.I change the value of WAKE_UP_THS, W...

Iakgu.1 by Associate III
  • 1047 Views
  • 1 replies
  • 0 kudos

Resolved! X-NUCLEO-CCA02M2 interface with nucleo-f401RE

Hi, I am using X-NUCLEO-CCA02M2 microphone board with nucleo-f401RE for USB audio streaming. Can anyone share the details about interfacing pin connection(which I2S pin is used)?. My understanding is like timer is used to connect pdm clock with I2S...

KK Y.1 by Associate II
  • 1838 Views
  • 1 replies
  • 0 kudos

Resolved! Allowed values for interrupt threshold of LIS2DH12

Hi, I am using a LIS2DH12 chip to detect the orientation(in 3D space) of a device.For this purpose I'm using the INT pins in 6D position mode to generate interrupt signal/s, that will alert me if the device has exited/entered a known positional area....

ilg by Associate
  • 1903 Views
  • 2 replies
  • 0 kudos

Resolved! High-pass path: BW_FILT setting

When BW_FILT[1:0] = 00, it's different between AN5201 AND DATASHEET. Which one is real?​in AN5201:In Datasheet(DocID031788):​​

0693W00000FBx7wQAD.png 0693W00000FBx8BQAT.png
user1 by Associate
  • 1107 Views
  • 1 replies
  • 0 kudos