MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I communicate via I2C on STEVAL-MKI159V1?

I'm using a Jetson Nano, and am trying to get it running though python. Extreme lack of documentation and references for the board has left be confused.Making the generic connections and running i2cdetect in the terminal, I detect the device at addre...

VVarm.1 by Associate
  • 1265 Views
  • 1 replies
  • 1 kudos

Resolved! Unico GUI C code generate option* using the .ucf file??

Hello ST,I am using the Unico 9.11.0.0 version software (STEVAL-MKI109V3 board) with STEVAL-MKI178V2 ( LSM6DSL ) Sensor board.from this link- https://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/configuration_examples/exampl...

0693W00000JNAbYQAX.png 0693W00000JNAbsQAH.png

Resolved! LSM9DS1 - how to set up interrupts for the magnetometer? Datasheet description of the INT_THS_L and INT_THS_H registers unclear.

The description of the threshold registers says: "The value is expressed in 15-bit unsigned. Even if the threshold is expressed in absolute value, the device detects both positive and negative thresholds.".There is only one threshold to be set, desp...

Resolved! Getting weird ISM330DHCX behavior during Increasing Temperature Test

Hello.I am trying to perform temperature calibration on ISM330DHCX (bought from adafruit) for both gyro and accel.IMU is sampled at 104Hz via SPI bus.The IMU sits inside a glass container, and is placed in a freezer. When the IMU temperature reaches ...

EMoso.1 by Associate
  • 2508 Views
  • 1 replies
  • 0 kudos

Resolved! Is the LIS3MDL 3-Axis Magnetometer suitable for my application?

Hi, I am looking into using the LIS3MDL 3-Axis Magnetometer in an application with high frequency oscillating magnetic fields. I have looked through the datasheet of the LIS3MDL and it seems to meet most requirements that I've checked. My application...

OSell.1 by Associate II
  • 2620 Views
  • 1 replies
  • 0 kudos

Resolved! No response from STEVAL-MKI109V3

Hi, I get no response from my computers when connecting the STEVAL-MKI109V3 with the USB cable. When connecting the cable the blue led turns on and after a few seconds the green led starts blinking. From what I read this is normal behaviour. The boar...

PJons.1 by Associate
  • 1385 Views
  • 2 replies
  • 0 kudos