MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unico GUI C code generate option* using the .ucf file??

Hello ST,I am using the Unico 9.11.0.0 version software (STEVAL-MKI109V3 board) with STEVAL-MKI178V2 ( LSM6DSL ) Sensor board.from this link- https://github.com/STMicroelectronics/STMems_Machine_Learning_Core/tree/master/configuration_examples/exampl...

0693W00000JNAbYQAX.png 0693W00000JNAbsQAH.png

Resolved! LSM9DS1 - how to set up interrupts for the magnetometer? Datasheet description of the INT_THS_L and INT_THS_H registers unclear.

The description of the threshold registers says: "The value is expressed in 15-bit unsigned. Even if the threshold is expressed in absolute value, the device detects both positive and negative thresholds.".There is only one threshold to be set, desp...

Resolved! Getting weird ISM330DHCX behavior during Increasing Temperature Test

Hello.I am trying to perform temperature calibration on ISM330DHCX (bought from adafruit) for both gyro and accel.IMU is sampled at 104Hz via SPI bus.The IMU sits inside a glass container, and is placed in a freezer. When the IMU temperature reaches ...

EMoso.1 by Associate
  • 2458 Views
  • 1 replies
  • 0 kudos

Resolved! Is the LIS3MDL 3-Axis Magnetometer suitable for my application?

Hi, I am looking into using the LIS3MDL 3-Axis Magnetometer in an application with high frequency oscillating magnetic fields. I have looked through the datasheet of the LIS3MDL and it seems to meet most requirements that I've checked. My application...

OSell.1 by Associate II
  • 2578 Views
  • 1 replies
  • 0 kudos

Resolved! No response from STEVAL-MKI109V3

Hi, I get no response from my computers when connecting the STEVAL-MKI109V3 with the USB cable. When connecting the cable the blue led turns on and after a few seconds the green led starts blinking. From what I read this is normal behaviour. The boar...

PJons.1 by Associate
  • 1366 Views
  • 2 replies
  • 0 kudos

How to read FIFO buffer data from lsm6dsox

Hi,we are trying to read FIFO buffer data but we are facing some issues in output data from FIFO can anyone help me regarding the FIFO register setting what is the value to be configured in the FIFO register?

Sprem.1 by Associate III
  • 6281 Views
  • 9 replies
  • 0 kudos

Resolved! ATWINC3400-MR210CA network controller driver for STM32?

Hi,I am student and we are using this Mikroe WiFi8 Click Board for one of our faculty projects. We are using STM32 Cube IDE, and we are using Clicker 2 for STM32 Development Board. I am trying to find suitable driver for this board. I only found Mikr...

ISaji.1 by Associate
  • 2503 Views
  • 1 replies
  • 0 kudos

LIS3DH: How to get FIFO watermark event signalled on INT1

I am struggeling to make the INT1 to activate due to a FIFO watermark event.I have a simple driver so far to ease the design verification testing of our card, and I am just trying to make sure that the INT1 line can be driven active by the LIS3DH.To ...

MVale.2 by Associate
  • 1675 Views
  • 2 replies
  • 0 kudos