MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

AIS2120 reading issue

volatile UB__8 ubAisRxData; volatile UB__8 ubSpiStatus = 0; void SPI_vInit(void) { disable_interrupts(); configure_D_OUT_SPI_MOSI_Pin(); // PTBDD_PTBDD5 = 1; // MOSI configure_D_IN_SPI_MISO_Pin(); //PTBDD_PTBDD4 = 0; // MISO c...

IIS3DWB High-Rate FIFO/DMA Data Transfer on STEVAL-STWINBX1

Hi all, I’m working on a project using the STEVAL-STWINBX1, and my main goal is to use the IIS3DWB vibration sensor as a high-speed vibrometer. I’m still pretty new to embedded programming (about 2 months in), so please bear with me! Project setup so...

Taha by Associate
  • 492 Views
  • 1 replies
  • 0 kudos

LSM6DSM high pass filter wake up interrupt

Hi,I am working on an accelerometer interrupt using the LSM6DSM. In AN4987 I found that I can configure the slope filter to use a window of WK_DUR samples that consecutively exceed WK_THS based on the given formula. I found good threshold settings fo...

Resolved! Bias stability of ISM330 and LSM6DSV

Hello,Could you provide the bias instability of ISM330DLC and LSM6DSV I could not find them in their datasheet ?Thank you by advance for your help

fgs by Associate II
  • 419 Views
  • 2 replies
  • 0 kudos

Problem with reading X-axis data from LIS2MDL

The measurement data of LIS2MDL was read in the application. Both the Y and Z axes were normal, and their data changed with the position. However, the data of the X axis was abnormal, and its value was the same as TEMP_OUT. Moreover, it was not relat...

微信图片_20250619220720_5.png