MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Is it possible to move from VL53L1X to VL53L1 ?

Hello, I have developped a product using VL53L1X last year, and recent communication from STM suggest there is an improvement in detection in a new product, VL53L1. I wonder if this is exactly the same product with only software improvement (hence I ...

GJour.1 by Associate II
  • 1449 Views
  • 1 replies
  • 0 kudos

Resolved! Problems with LIS3DSH, always receiving 0xFF

Hi,so a few months ago I wrote a program to read values from LIS3DSH sensor. It was working good until last week Z axis stopped working, and this week Y axis also. It always sends back 0x8080 values, while X axis is still working great. I have a cust...

bmak by Senior
  • 4049 Views
  • 8 replies
  • 0 kudos

Initialization error using STM32F4 with IMU by Bosch (BMI160)

Hi,I use STM32F4 with BMI160. But i have a problem. I cannot initiate BMI160 so I can not get gyro and accel data. You can see here my init functions:"init_sensor_interface();bmi160_init(&bmi160dev);init_bmi160_sensor_driver_interface();"When i write...

STEVAL-BCN002V1B Bluetooth-Connection to laptop

Hello ,Is it possible to connect the senor-borad STEVAL-BCN002V1B direct with our computer, if the computer has Bluetooth 5.0 standard. Or do I need an bluetooth extension board for my nucleo board.The aim is to read out the sensordata from the board...

FUhl.1 by Associate II
  • 1815 Views
  • 4 replies
  • 0 kudos

Resolved! Observing strange voltage ramp when VDD is above 2V - LSM6SOTR

We've just changed the way our system is powered: Previously the accelerometer was powered from a 1.8V regulator, now it's powered directly from a 3V coin cell (schematic part attached).With the change, we have started to observe a strange ramping wh...

OLewi.1 by Associate II
  • 4149 Views
  • 4 replies
  • 0 kudos

LIS3DH in FIFO mode gives garbage output

I'm trying to configure a LIS3DH to trigger INT1 after filling FIFO, after which I want to read out everything over I2C and then repeat.I've gotten it to work (at f=10 Hz, I get INT1 interrupts at the expected ~3 sec interval), but when I read out th...

BLind.3 by Associate
  • 1516 Views
  • 1 replies
  • 0 kudos

LPS22HH Atmospheric pressure strange temperature changes.

I started to evaluate LPS22HH using STEVAL-MKI109V3, STEVAL-MKI192V1, Pressure LPS22HH Kit, and Unico-GUI. Of the 4 STEVAL-MKI192V1 I purchased, the atmospheric pressure of 2 devices shows strange temperature changes.LPS22HH press =4.3268t+879.71[hpa...

tsuna by Associate II
  • 1661 Views
  • 1 replies
  • 0 kudos

Reading data asynchronously from I3G4250D

Hi all,I'm trying to read output data from a I3G4250D gyrometer, but despite everything I've done, I can't get rid of data corruption during asynchronous reads.The corruption seems to be caused by the registers being updated while we're reading data ...

0693W00000Kcu2sQAB.png
LPats.1 by Associate II
  • 1598 Views
  • 1 replies
  • 0 kudos